STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 302 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4120 Views
  • 0 replies
  • 3 kudos

GSM & STM32 file download via FTP

GSM modem is attached to STM32. Using FTP AT commands I am able to download a particular file from FTP server. Now I don't know where this downloaded file is saved inside the GSM modem. My goal is to transfer that file into STM32 and upgrade the firm...

sne_123 by Associate III
  • 2310 Views
  • 4 replies
  • 0 kudos

Loading Thread-CLI example on STM32WB

Hi,I am trying to evaluate Thread connectivity with my brand new STM32WB development kit using Thread_Cli_Cmd example. I connect the board NUCLEO-WB55.Nucleo to my PC via the ST-LINK connector then I run STM32Cubeprogrammer, did a full chip erase and...

WThal by Associate II
  • 1663 Views
  • 2 replies
  • 0 kudos

RSS_IMAGE_NOT_AUTHENTIC Wireless stack update error

Hello,I have STM32WB55 Nucleo kit (EPNWB55$CU5) from STM32WB workshop. As I know, it works only with special versions of wireless stack from workshop package.I tried to update USB dongle BLE stack with stm32wb5x_495B_wireless_cryp_BLE_Stack_fw_v1.0.0...

NMina by Associate
  • 739 Views
  • 0 replies
  • 0 kudos

STM32CubeMX do not support STM32WB IPCC Setting

The new STM32CubeMX 5.1.0 do not support STM32WB55 IPCC setting (System Core). Firmware STM32Cube_FW_WB_V1.0.0. I can not check the HandsOn's from the STM32WB55 Nucleo Board. The board is listed to the CubeMX.

AxelMC by Associate II
  • 4066 Views
  • 6 replies
  • 1 kudos

Resolved! STM32WB : Bug in FW_WB_V1.0.0: aci_gap_set_discoverable > hci_send_req > hci_cmd_resp_wait - wait infinitely for hci_cmd_resp_release after few connection/disconnection

In every example which i have tested after second device disconnection it stops Advertising. After a short investigation i found that aci_gap_set_discoverable waits for hci_cmd_resp_release. I don't know if problem is with stack on CM0 or it is pro...

WObre by Associate II
  • 1528 Views
  • 1 replies
  • 1 kudos

How to configure the RTC in stm32wb?

Hey everyone,I'm using a stm32wb55 nucleo board.When i'm using ST example about RTC, i have a problem with the accuracy of RTC and i want to know how i can configure RTC for increase her accurancy? I.E.: all of 10 minutes i lose 6 secondsThanks in ...

anoli by Associate
  • 1921 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.