STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 302 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4120 Views
  • 0 replies
  • 3 kudos

Thread_Coap_MultiBoard is not sending Traces

I would like to get the traces of the Thread_Coap_MultiBoard Application to read the CoAP-Messages that are transmitted/received. I connected a tested USB-UART adapter to CN10 (35 + 37) and the terminal is running at 115200 8N1N. I already tried to s...

david.i by Associate
  • 844 Views
  • 1 replies
  • 0 kudos

I-CUBE-LRWAN ADC reading not working

Hi,I use the I-CUBE-LRWAN code in the B-L072Z-LRWAN1.When I want to read an ADC channel I use to read pin PA5:a = HW_AdcReadChannel(ADC_CHANNEL_5);And to read ADC channel PA4 I use:a = HW_AdcReadChannel(ADC_CHANNEL_4);By using the mlm32l0xx_hw.c.But ...

Nvan.9 by Associate II
  • 1514 Views
  • 2 replies
  • 0 kudos

B-L072Z-LRWAN1 Stop mode example?

Hi,I am using B-L072Z-LRWAN1 and I-Cube-LORAWAN SDK specifically AT_Slave project. I am trying to put device in Stop mode but I can see it exist from stop mode immediately.How can I put some condition for device to exit from stop mode or not? Are th...

S.M. by Associate II
  • 724 Views
  • 0 replies
  • 0 kudos

B-L072Z-LRWAN1 Current Consumption

Hi,I am using B-L072Z-LRWAN1 and AT_Slave project from I-Cube-LRWAN. Can Anyone help me with the setup to measure current consumption like jumper position and across which pins to measure current?Thank You

S.M. by Associate II
  • 1024 Views
  • 1 replies
  • 0 kudos

Recommendation for matching network

Hello All,I'm planing to use a STM32WB55C on a design and I have the choice to either use an old-fashioned Pi matching network + Filter or use an integrated MN/Filter (MPLF-WB55-01E3).Knowing that the part have 0 stock (some expected in a few weeks o...

rnone by Associate II
  • 712 Views
  • 0 replies
  • 0 kudos

Resolved! AN3359 unit ???

Hello,Concerning the AN3359, what is the unit of the figure 2 ?Thanks.

LVent by Associate II
  • 2608 Views
  • 2 replies
  • 0 kudos

Resolved! Why can't I download STM32CubeWB?

STM32CubeWB is the firmware package of the stm32wb series.when i clicked the Get Software Button,the page jumped to the home page.I have logged in to my ST Account.

�??bo by Associate
  • 2180 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.