2019-07-24 12:10 PM
I follow steps 1-5 for the Release Notes for STM32WB Copro Wireless Binaries (STM32CubeWB 1.1.1 patch):
./STM32_Programmer_CLI -c port=usb1 -fwdelete
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in FS Mode
SN : 206B38933036
FW version : 0x011a
Device ID : 0x0495
Device name : STM32WBxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M0+/M4
RSS state is RSS_ERROR
RSS status is RSS_NOT_RUNNING
RSS state is RSS_IDLE
RSS status is RSS_NO_ERROR
Deleting firmware ...
Firmware delete finished
fwdelete command execution finishedThen I check the FUS version:
./STM32_Programmer_CLI -c port=usb1 -r32 0x20030030 1
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in FS Mode
SN : 206B38933036
FW version : 0x011a
Device ID : 0x0495
Device name : STM32WBxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M0+/M4
0x20030030 : 00050300Then I proceed to update the FUS:
./STM32_Programmer_CLI -c port=usb1 -fwupgrade stm32wb5x_FUS_fw.bin 0x080EC000 firstinstall=0
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in FS Mode
SN : 206B38933036
FW version : 0x011a
Device ID : 0x0495
Device name : STM32WBxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M0+/M4
RSS state is RSS_IDLE
RSS status is RSS_NO_ERROR
Old Firmware delete ...
Deleting firmware ...
Error: Device has been disconnected
Segmentation fault (core dumped)Now nothing works! Any command results in a segmentation fault. As you can see from the code snippets I'm using STM32CubeProgrammer.
Solved! Go to Solution.
2019-07-27 11:09 AM
This seems to be a bug with STM32_Programmer_CLI Linux version. Where can I submit a bug report? Windows is working fine but we require running Linux on our production systems.
2019-07-24 12:48 PM
I tested the same nucleo dongle on Windows, and managed to update the FUS and the wireless coprocessor binary successfully.
For the system that gave the errors, I was using:
Linux Mint 19.1
Kernel 4.15.0-54
2019-07-27 11:09 AM
This seems to be a bug with STM32_Programmer_CLI Linux version. Where can I submit a bug report? Windows is working fine but we require running Linux on our production systems.
2019-08-14 4:05 AM
Please try firstinstall=1 instead, it should work better
Actually this option shall be set to 1 in the case of FUS anyway, because you cannot delete the existing FUS version prior to installing new one.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.