2019-05-23 3:56 AM
Hi All;
I am use I-CUBE-LRWAN version 1.2.1. I am program in class C mode. I send a message downlink from network server and I checked that the data was actually sent out. Why I can't received a message downlink immediately. Could you please advice me?
Thank you,
Best regards.
Solved! Go to Solution.
2019-08-15 2:08 AM
Hi,
I have noticed the same problem using End_Node example. I have changed APP_TX_DUTYCYCLE to 900000 (15min) and LORAWAN_DEFAULT_CLASS to CLASS_C
5-7 min after uplink message, downlink message is received .After that and before next uplink, downlink messages don't get received.
I have tested this with B-L072Z-LRWAN1 and own HW-designs with i-cube_LRWAN 1.2.1 based FW and CMWX1ZZABZ-091 radio.
There is also problem with receiving JoinAccept messages, which might relate to downlink receive problems. The end mode might require 2-3 JoinRequire/JoinAccept messages before it has really joined the network.
BR,
Timo
2019-08-15 2:08 AM
Hi,
I have noticed the same problem using End_Node example. I have changed APP_TX_DUTYCYCLE to 900000 (15min) and LORAWAN_DEFAULT_CLASS to CLASS_C
5-7 min after uplink message, downlink message is received .After that and before next uplink, downlink messages don't get received.
I have tested this with B-L072Z-LRWAN1 and own HW-designs with i-cube_LRWAN 1.2.1 based FW and CMWX1ZZABZ-091 radio.
There is also problem with receiving JoinAccept messages, which might relate to downlink receive problems. The end mode might require 2-3 JoinRequire/JoinAccept messages before it has really joined the network.
BR,
Timo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.