2019-08-16 5:55 AM
Hi !
I got a discovery board B-L072cz-LRWAN1. It go to stop mode and when the Alarm trig it wake up and run the program correctly. But when I use the uart for print or anything else, the program stop.
Here is my code. It's based on the cube-LRWAN1 example :
int main()
{
HAL_Init( );
SystemClock_Config( );
DBG_Init( );
HW_Init( );
while(1)
{
PRINTF("Sleep\r");
SX1276SetSleep();
HAL_Delay(200);
stm32l_lowPowerSetup();
stm32l_lowPowerResume();
PRINTF("Wake\r");
}
}
void stm32l_lowPowerSetup(void)
{
__HAL_RCC_PWR_CLK_ENABLE(); // Enable Power Control clock
HAL_PWREx_EnableUltraLowPower(); // Ultra low power mode
HAL_PWREx_EnableFastWakeUp(); // Fast wake-up for ultra low power mode
// Disable Unused Gpios
_stm32l_disableGpios(); // Disable GPIOs based on configuration
HW_RTC_SetAlarm(10000);
// Switch to STOPMode
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
}
void stm32l_lowPowerResume(void)
{
HAL_Init( );
SystemClock_Config( );
HAL_RTC_MspInit(&hrtc);
DBG_Init( );
HW_Init( );
HAL_UART_MspInit(&huart2);
}
void HAL_UART_MspInit(UART_HandleTypeDef *huart)
{
static DMA_HandleTypeDef hdma_tx;
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* Enable GPIO TX/RX clock */
USARTx_TX_GPIO_CLK_ENABLE();
USARTx_RX_GPIO_CLK_ENABLE();
/* Enable USARTx clock */
USARTx_CLK_ENABLE();
/* Enable DMA clock */
DMAx_CLK_ENABLE();
/*##-2- Configure peripheral GPIO ##########################################*/
/* UART pin configuration */
vcom_IoInit();
/*##-3- Configure the DMA ##################################################*/
/* Configure the DMA handler for Transmission process */
hdma_tx.Instance = USARTx_TX_DMA_CHANNEL;
hdma_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_tx.Init.Mode = DMA_NORMAL;
hdma_tx.Init.Priority = DMA_PRIORITY_LOW;
#ifndef STM32L152xE
hdma_tx.Init.Request = USARTx_TX_DMA_REQUEST;
#endif
HAL_DMA_Init(&hdma_tx);
/* Associate the initialized DMA handle to the UART handle */
__HAL_LINKDMA(huart, hdmatx, hdma_tx);
/*##-4- Configure the NVIC for DMA #########################################*/
/* NVIC configuration for DMA transfer complete interrupt (USART1_TX) */
HAL_NVIC_SetPriority(USARTx_DMA_TX_IRQn, USARTx_Priority, 1);
HAL_NVIC_EnableIRQ(USARTx_DMA_TX_IRQn);
/* NVIC for USART, to catch the TX complete */
HAL_NVIC_SetPriority(USARTx_IRQn, USARTx_DMA_Priority, 1);
HAL_NVIC_EnableIRQ(USARTx_IRQn);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.