NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I am working with an STM32WB55RGV6 on a custom board powered by battery (always connected).I successfully ran the Proximity example (non-RTOS) with BLE stack before, but after I worked on another project that used BLE stack + FreeRTOS, the BLE ...
Hello, I am developing a Sleepy End-Device based on STM32WB5MMG which should read and transmit sensor data periodically. The board is mounted to a PCB with the recommended layout for optimal antenna gain. The sensor readings are transmitted with a cu...
Hello @STTwo-32,I was having the same issue and pressing the "start wireless stack" button did the trick for me. I was assuming after flashing the FUS & BLE Stack firmware, is that the CPU2 would be up and running already. So, does this mean that we ...
Hello!I have an STM32WB5MMG with a breakout board (more specifically Sparkfun ATP breakoutSparkFun MicroMod ATP Carrier Board - DEV-16885 - SparkFun Electronicswith the STM32WB5MMG module SparkFun MicroMod STM32WB5MMG Processor - DEV-21438 - SparkFun...
Hi everyone , I'm testing ultra-low power on the NUCLEO-WL55JC using STM32CubeIDE . My goal is to reach ~0.9 µA in Stop 2 mode, but I consistently measure around 2.9 mA, even with the debugger disconnected. My setup: Stop 2 mode enabled MSI @ 100 kHz...
Hello,I am having an issue with my STM32WBA65MI-based project file (IOC file) and CubeMX (6.15.0). It also happens when configuring the IOC file in CubeIDE 1.19.0.When I configure the clocks and then generate code and save the IOC file and then close...
Greetings,This is my frist time with wireless mcu. I just want to ask whether RTC is required for LORA Sub GHz Phy communication ? Any help will be greatful.
Hello,I'm having trouble building a LoRaWAN project targeting the STM32WLE5JCI6. The same error occurs even on a clean, newly created project, which leads me to believe there might be a compatibility issue between the IDE and the software package.■ T...
Hello everybody,For a proof of concept, I attempted to validate the LoRa modulation by having two B-WL5M-SUBG1 boards exchange ping-pong messages. However, I couldn't manage to exchange data with these boards at a distance greater than 230m in an ope...
We would like to power the VDD33 domain of an STM32WB0 device (STM32WB05KZ) from an external 3.3V source and the other domains from an external 1.8V source. In theory, it should be possible - by supplying 1.8V to VDDSD in SMPS BYPASS mode, or directl...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.