STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WL3 status when wakeup from deep sleep not working

1. [Part Number] STM32WL33CC12. [Environment] Windows OS, STM32CubeIDE version 1.18.0, Firmware package STM32Cube FW_WL3 V1.1.03. [Schematics] STM32 Nucleo-64 development board4. [Details] See below.5. [Expected behavior] When the device is woken up ...

ola by Associate III
  • 3280 Views
  • 7 replies
  • 4 kudos

Resolved! How to connect the 2 stm32wb55rev6 boards through ble?

I am using the stm32wb55rev6 boards for the ble.What should be the configuration to commuicate between the 2 stm32wb55rev6 boards?i am using the trasparent mode in 1 stm32wb55rev6 board and what should be the configuration on the other board to scan ...

TejasK by Associate III
  • 388 Views
  • 1 replies
  • 0 kudos

Feedback on STM32WB55 Series Flash Architecture

My Feedback on STM32WB Series Flash ArchitectureDear STMicroelectronics Team,As an experienced developer working  with the STM32WB series, I must voice a critical concern about its current flash memory architecture.By placing both the Cortex‑M4 appli...

islavv by Associate III
  • 593 Views
  • 1 replies
  • 0 kudos

Resolved! not able to connect to the stm32cube monitor rf.

i am usng stm32wb55rev6 microcontroller for my project. I updated the firmware upgrade service to the latest version of the v2.1.0.0 and updated the stack version to the latest version of v1.23.0.3.Still i am not able to connect to the stm32cube moni...

TejasK_0-1755520705766.png TejasK_1-1755520723599.png
TejasK by Associate III
  • 1822 Views
  • 7 replies
  • 0 kudos

FUS_IMAGE_ERSERROR from FUS while FW upgrade

Hi there,On a STM32WB55RG, I would like to write a routine in my firmware to upgrade the wireless firmware through the FUS mailbox.I'm able to exchange request/response through the mailbox, for instance, at startup FUS_GET_STATE returns FUS_STATE_IDL...

rmedaer by Associate II
  • 967 Views
  • 6 replies
  • 0 kudos

STM32 WL55JC1 FUOTA

Good morning, I have been trying to integrate FUOTA for a few days in my Nuclo STM32 WL55JC1 project. Starting from the provided example STM32CubeWL_FW_1.3.1 from MXCube, if I try to build in CubeIDE I get the following error:   make[1]: *** No rule ...

IngSerio by Associate III
  • 2101 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.