NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am trying to reconfigure the BLE_HID application to the smallest STM32WBCC processor.The linker script for BLE_Hid example with STM32WBRG which look like this ( stm32wb55xx_flash_cm4.ld) /* Highest address of the user mode stack */_estack = 0x2...
When programming a binary file stm32wb5x_FUS_fw into the STM32WB55CC, after the line "RSS Status is RSS_IMAGE_IS_NOT_AUTHENTIC" appears a line "Error: fireware not authentic" in red. Why could an error like that happen and why it is impossible to pro...
Try to get demo firmware sources for USB dongle MB1293C. Also a .hex file will be useful.I am trying to use STM32Cube utility to generate code from the .ioc file but the code generated does not support the usb driver properly. Any hints to how to get...
The original version of STM32WB Ble stack is 1.0.0.3/e, Other releases include 1.0.0, 1.1.0, 1.1.1, 1.2.0. What are the differences between these versions? Can you provide detailed documentation?In addition, I'm going to buy some STM32WB . Are these ...
You can find it here : http://risinghf.com/#/product-details?product_id=26&lang=en
I see that cubemx shows x-cube-ble1 as an available sw package for a stm32wb55 project. Is it possible to use the x-cube-ble1 stack on the wb series? I'm having a hard time in getting the flow of how a ble app is configured on the wb, in this forum ...
I'm developing a custom board with STM32WB55CGU6 with firmware based on Cable Replacement example. Trying changing the advertised name, I can not put more than 5 chars, the BLE stops working. I know the standard advertising supports until 7 chars. Wh...
So we update the FUS following the steps specificed in the release note, the process went ok and the FSU was upgradedUSB speed : Full Speed (12MBit/s) Manuf. ID : STMicroelectronics Product ID : DFU in FS Mode SN : 206936933136 FW versi...
In application note AN5289 page 35 it is written that you need to wait for the connection to be established and then call aci_gap_set_pairing_req(). I call this function when connection established event happens, but when I do this return status is 0...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.