2019-10-15 10:50 AM
In STM32CubeProgrammer I can set RDP on AA level and BB level, but in CLI mode read/write protection is constantly in BB. In CLI protection byte doesnt change, I mean I can't change it
and can't write FUS or stack, and even check the fuse version.
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=usb1 -rdu
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in FS Mode
SN : 207D308E3036
FW version : 0x011a
Device ID : unknown
Warning: Device is under Read Out Protection
Disabling memory Read Protection...
Memory Read Protection disabled successfully
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=usb1 -rdu
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in FS Mode
SN : 207D308E3036
FW version : 0x011a
Device ID : unknown
Warning: Device is under Read Out Protection
Disabling memory Read Protection...
Memory Read Protection disabled successfully
2019-10-15 10:54 AM
More action
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=usb1 -r32 0x20030030 1
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in FS Mode
SN : 207D308E3036
FW version : 0x011a
Device ID : unknown
Warning: Device is under Read Out Protection
Error: RDP level is set to 1 (0xBB), try using Read UnProtect (-rdu) command in order to remove the Read Out Protection.
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=usb1 -fwdelete
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in FS Mode
SN : 207D308E3036
FW version : 0x011a
Device ID : unknown
Warning: Device is under Read Out Protection
Error: fwdelete command is not supported for such device
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.