NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi there,I am working on Murata cmwx1zzabz (i.e. STM32L072CZ) and my code is based on the ST en.i-cube_lrwan. For all the basic stuff (joining, sending messages) it runs fine. The Mac commands, that actually manage the network, are OK except the "sti...
How change mbed linker for STM32WB55 to used STM_OTA bootloader (need to add TAG_OTA_START, TAG_OTA_END ...). This is my code but don't work, mbed given my error:; #if !defined(MBED_APP_START) ; #define MBED_APP_START 0x08000000 #define MBED_APP_STAR...
I'm using ST-LINK of p-nucleo-wb55 board. I tried to connect P-Nucleo-wb55 to the ST-LINK Utility, but I can't. Below the comment of ST-LINK Utility.11:09:19 : ST-LINK SN : 0671FF39373842504306602511:09:19 : ST-LINK Firmware version : V2J35M2611:09:1...
I am new to STM32WB, i have written BLE middle-ware application it is working on Scheduler, in main while Loop SCH_Run(~0) is handlling the entire middleware, now i want to wirte the actual application for Cortex-M4 but when i add anything in the Whi...
Is there a possibility to use the STM32WBxx with wifi? I know it can handle bluetooth or zigbee.Or maybe is there in the near future a firmeware upgarde to use wifi?Thanks!
According to manual I should getFast channels: 0.234 μs for 12-bit resolution (4.27 Ms/s)Slow channels: 0.297 μs for 12-bit resolution (3.37 Ms/s)but I am getting only get 2Ms/s.I am clocking the chip at 64MHz and using P-NUCLEO-WB55 evaluation board...
The Gateway uses the Semtech SX1301 / SX1257 Chipsatzdesign, LoRa frequencies 863 - 870 MHz (EU)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.