STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 302 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4120 Views
  • 0 replies
  • 3 kudos

Is GPIO control disabled when using Input Capture?

Hello.I am trying to do single-channel touch-sensing without using the TSC. For that, I put a weak pull-up on that pin. In a cyclic process, I make the pin OUTPUT-LOW, then release it and measure the rise time through Input Capture. It's a very basic...

abbas14 by Associate II
  • 2077 Views
  • 3 replies
  • 0 kudos

Thread UDP send example for STM32WB

I want to use the OpenThread UDP API. So far I implemented the UDP datagram reception without any problems. Sending a datagram using the CLI works fine. When it comes to sending a datagram via the API I always get either OT_ERROR_INVALID_SOURCE_ADDRE...

Resolved! OpenOCD source code.

Is there any place I can find the source code for OpenOCD bundled with current release of STM32CubeIDE? I'm asking because I think source for this should be provided as it is under GPL, I'm asking since STM32WB is not supported in source available o...

ChrisH by Associate III
  • 3665 Views
  • 4 replies
  • 1 kudos

Need help programming STM32WB55CEU6 CPU2 BLE firmware.

Hi, I have in hand a customer board with a STM32WB55CEU6 MCU. I was able to program CPU1 (M4) firmware but it seem that CPU2 (M0+) didn't have any firmware programmed.I have found that I need to program stm32wb5x_BLE_Stack_fw.bin into CPI2. Did you h...

MDrou by Associate
  • 906 Views
  • 1 replies
  • 0 kudos

Theoretical current consumption calculation STM32WB

We are currently working on STM32WBCC. Let's say my device name is DEVA. Have the following questions:1. DEVA needs any ability to connect to another BLE device DEVB.2. DEVA needs to maintain the lowest possible power when having the connection in ta...

STHIL.1 by Associate
  • 704 Views
  • 0 replies
  • 0 kudos

STM32WB55 nucleo board BLE STACK problem

i have been Using STM32WB55 Nucleo Board , and have successfully implemented BLE examples from repository and its Working fine, but suddenly now my board is not executing any BLE Applications , so i have updated M0 Cortex firmware i.e BLE stack From ...

DMist by Associate II
  • 1168 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.