2019-11-18 11:44 AM
Is there any place I can find the source code for OpenOCD bundled with current release of STM32CubeIDE? I'm asking because I think source for this should be provided as it is under GPL, I'm asking since STM32WB is not supported in source available on SF and I want to compile everything from scratch.
Solved! Go to Solution.
2019-11-19 5:26 AM
Hi Chris,
At ST level we are aware that the code should be public, that's why we are upstreaming our contributions into the official OpenOCD git.
For example the STM32WB support is here: http://openocd.zylin.com/#/c/4933/
but this change is not merged yet in the master branch.
Furthermore, we have a mirror of OpenOCD hosted here: git://git.ac6.fr/openocd
this mirror already contains the support of STM32WB in the branch named "st".
In the near future, we will host, another mirror into Github, representing the ST official fork of OpenOCD.
You can use the mirror above, until we prepare the Github mirror.
You will be notified once the Github mirror is ready.
Regards,
Tarek
2019-11-19 2:14 AM
openocd-code> git remote -v
origin https://git.code.sf.net/p/openocd/code (fetch)
origin https://git.code.sf.net/p/openocd/code (push)
2019-11-19 5:26 AM
Hi Chris,
At ST level we are aware that the code should be public, that's why we are upstreaming our contributions into the official OpenOCD git.
For example the STM32WB support is here: http://openocd.zylin.com/#/c/4933/
but this change is not merged yet in the master branch.
Furthermore, we have a mirror of OpenOCD hosted here: git://git.ac6.fr/openocd
this mirror already contains the support of STM32WB in the branch named "st".
In the near future, we will host, another mirror into Github, representing the ST official fork of OpenOCD.
You can use the mirror above, until we prepare the Github mirror.
You will be notified once the Github mirror is ready.
Regards,
Tarek
2019-11-19 9:07 AM
Hi Tarek,
thanks for clarifying that, I noticed on zylin there were references to STM32WB but wasn't sure if that were commits from ST. Sourceforge is quite outdated and I noticed a lot of open pull requests on zylin which aren't merged so I assumed you must have an alternative repo. Thanks for AC6 address!
Regards
Chris
2020-01-13 5:16 AM
Hi Chris,
A new repository is available under https://github.com/STMicroelectronics/OpenOCD
STMicroelectronics is actively working at merging these modifications in the official OpenOCD. In the mean time, these modifications are available in this repository.
This repository will be synchronized with STM32CubeIDE releases.
Regards,
Tarek
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.