2019-05-13 3:04 AM
Good morning everyone,
I'm coding with Atollic Truestudio and CubeMX.
I would like to ask for some helps concerning a function called "arm_bitreversal_32" in the "arm_cfft_f32.c".
Here is my problem.
I'm trying to use the function "arm_cfft_f32(x,x,x,x)" from the "arm_cfft_f32.c" file. And I got this error in this C file:
I'm not sure if some files are missed or I should implement it by myself because the function "arm_bitreversal_32()" is declare externally (extern void arm_bitreversal_32()).
I thank everyone who will try to help me to resolve my error.
arm_cfft_f32.c":
#include "arm_math.h"
#include "arm_common_tables.h"
extern void arm_radix8_butterfly_f32(
float32_t * pSrc,
uint16_t fftLen,
const float32_t * pCoef,
uint16_t twidCoefModifier);
extern void arm_bitreversal_32(
uint32_t * pSrc,
const uint16_t bitRevLen,
const uint16_t * pBitRevTable);void arm_cfft_f32(
const arm_cfft_instance_f32 * S,
float32_t * p1,
uint8_t ifftFlag,
uint8_t bitReverseFlag)
{
uint32_t L = S->fftLen, l;
float32_t invL, * pSrc;
if(ifftFlag == 1u)
{
/* Conjugate input data */
pSrc = p1 + 1;
for(l=0; l<L; l++)
{
*pSrc = -*pSrc;
pSrc += 2;
}
}
switch (L)
{
case 16:
case 128:
case 1024:
arm_cfft_radix8by2_f32 ( (arm_cfft_instance_f32 *) S, p1);
break;
case 32:
case 256:
case 2048:
arm_cfft_radix8by4_f32 ( (arm_cfft_instance_f32 *) S, p1);
break;
case 64:
case 512:
case 4096:
arm_radix8_butterfly_f32( p1, L, (float32_t *) S->pTwiddle, 1);
break;
}
if( bitReverseFlag )
arm_bitreversal_32((uint32_t*)p1,S->bitRevLength,S->pBitRevTable);
if(ifftFlag == 1u)
{
invL = 1.0f/(float32_t)L;
/* Conjugate and scale output data */
pSrc = p1;
for(l=0; l<L; l++)
{
*pSrc++ *= invL ;
*pSrc = -(*pSrc) * invL;
pSrc++;
}
}
}main.c:
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32wbxx_hal.h"
#include "arm_math.h"
#include "arm_common_tables.h"
#include "arm_const_structs.h"
#include <math.h>
/* Global variables */
/* Global define */
#define SAMPLE_FREQUENCY_UNDEC 1024 // A ajuster selon la frequence de la porteuse
#define SAMPLE_TIME_UNDEC (float) 1.0/SAMPLE_FREQUENCY_UNDEC
#define SAMPLES_UNDEC (int) 8*SAMPLE_FREQUENCY_UNDEC /* 8 secondes au total */
/* Decimation define */
#define NUMTAPS (uint16_t) 31 // Order(30) + 1
#define M (uint8_t) 32 // Divise SAMPLE_FREQ_UNDEC. Limite max : M < VIBE_SAMPLE
#define BLOCKSIZE (uint32_t) 64
#define NUMBLOCKS (uint32_t) SAMPLES_UNDEC/BLOCKSIZE
/* FFT define */
#define FFT_SIZE SAMPLES_UNDEC/M
/* Simulation define */
#define CARRIER_FREQUENCY 256 // Attention multiple de 2 pour que SAMPLE_FREQUENCY multiple de CARIIER_FREQUENCY afin que VIBE_SAMPLES soit entier
#define CARRIER_SIZE (int) SAMPLE_FREQUENCY_UNDEC/CARRIER_FREQUENCY
#define MODUL_FREQUENCY 1
#define VIBE_FREQUENCY (int) 0.1*CARRIER_FREQUENCY
#define VIBE_SAMPLES (int) (SAMPLE_FREQUENCY_UNDEC/CARRIER_FREQUENCY)*(VIBE_FREQUENCY) // Multiple de 1/CARRIER_FREQUENCY, durée 0;01 s. Durée minimale = 1/CARRIER_FREQUENCY; durée max = 1/MODUL_FREQUENCY
#define MODUL_SIZE (int) SAMPLE_FREQUENCY_UNDEC/MODUL_FREQUENCY
#define SIM_SIZE (int) MODUL_SIZE
/* Decimation settings */
const float32_t firCoeffs[NUMTAPS] = {0.0035214853,0.004185653,0.005849378,0.008574021,0.012351584,0.017101394,0.022671906,0.028847635,0.035360847,0.041907296,0.048164908,0.053814158,0.058558714,0.06214481,0.064378045,0.065136336,0.064378045,0.06214481,0.058558714,0.053814158,0.048164908,0.041907296,0.035360847,0.028847635,0.022671906,0.017101394,0.012351584,0.008574021,0.005849378,0.004185653,0.0035214853};
static float32_t firState[NUMTAPS + BLOCKSIZE - 1];
static float32_t undecimatedSignal[SAMPLES_UNDEC];
static float decimatedSignal[SAMPLES_UNDEC/M];
static float32_t *pDecimatorInput, *pDecimatorOutput;
/* FFT settings */
static float fftInput[FFT_SIZE*2]; // Initialize with zeros
static float fftOutput[FFT_SIZE]; // Initialize with zeros
static float maxValue; // Max FFT value is stored here
static uint32_t maxIndex; // Index in Ouput arraywhere max value is
/* Define simulation settings */
float carrier[CARRIER_SIZE];
float modul[MODUL_SIZE];
float sim[SIM_SIZE];
/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
RTC_HandleTypeDef hrtc;
TIM_HandleTypeDef htim16;
UART_HandleTypeDef huart1;
PCD_HandleTypeDef hpcd_USB_FS;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ADC1_Init(void);
static void MX_TIM16_Init(void);
static void MX_RTC_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_USB_PCD_Init(void);
/* Functions */
/* Create the carrier buffer */
void calculate_carrier(){
for(int i = 0; i < CARRIER_SIZE; i += 1){
float t = i * SAMPLE_TIME_UNDEC;
float phase = 2 * PI * CARRIER_FREQUENCY * t;
carrier[i] = sin(phase);
}
}
/* Create the modulator buffer */
void calculate_modulator(){
for(int i = 0; i < VIBE_SAMPLES; i += 1){
modul[i] = 1.0;
}
for(int i = VIBE_SAMPLES; i < MODUL_SIZE; i += 1){
modul[i] = 0.0;
}
}
/* Calculate the sim signal */
void calculate_sim(){
calculate_carrier();
calculate_modulator();
for(int i= 0; i < SIM_SIZE; i += 1){
int i_size = ((float) i) / CARRIER_SIZE;
int i_carrier = i - CARRIER_SIZE * i_size;
sim[i] = 0.5 * modul[i] * carrier[i_carrier] + 0.5;
}
}
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
MX_TIM16_Init();
MX_RTC_Init();
MX_USART1_UART_Init();
MX_USB_PCD_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* DAC record */
for(int i = 0; i < SAMPLES_UNDEC; i += 1){
HAL_Delay(SAMPLE_TIME_UNDEC);
HAL_ADC_Start(&hadc1);
if(HAL_ADC_PollForConversion(&hadc1, 5) == HAL_OK)
{
undecimatedSignal[i] = abs(HAL_ADC_GetValue(&hadc1) - 0.5f);
}
}
/* Decimation */
arm_fir_decimate_instance_f32 S;
arm_fir_decimate_init_f32(&S, NUMTAPS, M, &firCoeffs[0], &firState[0], BLOCKSIZE );
pDecimatorInput = &undecimatedSignal[0];
pDecimatorOutput = &decimatedSignal[0];
for(int i = 0; i < NUMBLOCKS; i ++){
arm_fir_decimate_f32(&S, pDecimatorInput + (i * BLOCKSIZE), pDecimatorOutput + (i * BLOCKSIZE/M), BLOCKSIZE);
}
/* Init FFT */
float meanDecimatedSignal;
arm_mean_f32(decimatedSignal, SAMPLES_UNDEC/M, &meanDecimatedSignal);
for(int i = 0; i < 2 * FFT_SIZE; i += 2){
fftInput[i] = decimatedSignal[i/2] - meanDecimatedSignal;
fftInput[i+1] = 0;
}
if(FFT_SIZE == 1024){
arm_cfft_f32(&arm_cfft_sR_f32_len1024, fftInput, 0, 1);
}else if(FFT_SIZE == 512){
arm_cfft_f32(&arm_cfft_sR_f32_len512, fftInput, 0, 1);
}else if(FFT_SIZE == 256){
arm_cfft_f32(&arm_cfft_sR_f32_len256, fftInput, 0, 1);
}else if(FFT_SIZE == 128){
arm_cfft_f32(&arm_cfft_sR_f32_len128, fftInput, 0, 1);
}
/* Compute FFT and max value */
arm_cmplx_mag_f32(fftInput, fftOutput, FFT_SIZE);
arm_max_f32(fftOutput, FFT_SIZE/2, &maxValue, & maxIndex);
/* FFT Result */
float freqStep = (SAMPLE_FREQUENCY_UNDEC/((float)M) / ((float)FFT_SIZE));
float maxFreq = maxIndex * freqStep;
HAL_UART_Transmit(&huart1, "maxFreq", strlen("maxFreq"), 10);
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
2019-05-31 12:22 AM
Hello,
can someone help me with this problem?
2020-01-12 8:37 PM
Seven months have passed and I don't know if you still need help,I have the same problem as you,but i didn't use cubex,
The arm_radix8_butterfly_f32 is in the "arm_cfft_radix8_f32.c" which under the CMSIS/5.6.0/CMSIS/DSP/Source/TranformFunctions folder .And the arm_bitreversal_f32 is in the same folder ——"arm_bitrevesal.c" .That means you need to add them separately.
Good Luck
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.