STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 302 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4120 Views
  • 0 replies
  • 3 kudos

Problem in write characteristic of p2p_client_app.c STM32WB55

Hello! I can not send more that 3 bytes from client to server using the write characteristic(aci_gatt_write_without_resp) in BLE_p2p_client_app.c . When I change CharValueLetgh to something higher then 3 my board cannot notify anymore. How can I solv...

Kolab by Senior
  • 801 Views
  • 1 replies
  • 0 kudos

FUS UPDATE ISSUE

In my recent received P-Nucleo-MB1355C board, it has FUS version FUSv0.5.3, which need to upgraded with newer version available in STM32Cube_FW_WB_V1.4.0. While trying to update with -fwupgrade command, getting error Error: Firmware not authentic! ....

0690X00000DXBGXQA5.png
PS.2 by Associate II
  • 2438 Views
  • 15 replies
  • 0 kudos

How to transfer data between two STM32+SX1272 LoRa module

Hello everyone. I am debugging the STM32+SX1272 LORA wireless communication. Now I follow the sample code provided by ST company which download from the website. The sample code version is STM32CubeExpansion_LRWAN_V1.3.1. Now I can transfer "ping" a...

mlau.18 by Associate II
  • 1732 Views
  • 1 replies
  • 0 kudos

P-Nucleo-LRWAN2 + I-CUBE-LRWAN V1.3.1

I am a newbie on Lora and recently I bought a P-Nucleo-LRWAN2 development kit to start my projects using Lora communication technology.As soon as I received the development boards I follow the instruction on the manual and I successfully connected th...

AFerr.41 by Associate II
  • 775 Views
  • 0 replies
  • 2 kudos

I2C accessing peripheral with 32 bit address register

I have connected a peripheral to STM32WB via I2C,.The functions HAL_I2C_Mem_Write() and I2C, HAL_I2C_Mem_Read() are designed for upto 16 bit register address. (The function checks if MemAddSize is 8 bit or 16 bit).Do I have to rewrite the implementat...

0693W000000X1mRQAS.png
HSing by Associate II
  • 2313 Views
  • 2 replies
  • 0 kudos

WB55 Nucleo BLE - Connection issues

When I load the handson_2 everything works fine. However when i open a new project and initialize it as a p2p server application - And follow the steps in handson_2 training video, I can get my nucleo to advertise just fine - however I cannot connect...

Soepoe by Associate II
  • 1130 Views
  • 1 replies
  • 0 kudos

Best Development Kit for Basic LoRa implementation

Hi there!I've used STM32's for years, and am a huge fan. I now want to broaden my experience into LoRa (I have experience with Wi-Fi, Bluetooth, and even ST's SPSGRF range). I saw at the start of the year there was some news about ST's own chip which...

SWill.10 by Associate II
  • 1426 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.