2020-04-05 10:58 PM
Enable Ble Extended data packet(Send 251 Bytes in one Time) support.
* Data of 249 bytes is send and receive successfully but data of 250 and 251 Bytes not send and receive.
2020-04-29 8:58 AM
Could you be more explicit on the way to try to extend it?
What function did you use? For which kind of packet do you want to extend the data payload?
2020-05-09 5:25 AM
ble max data Throughput , As-
.) connection complete
/* Extended Packet Support */
hci_le_set_data_length(connection_complete_event->Connection_Handle, 251, 0x0848);
.) change p2p notify characteristic size -
aci_gatt_add_char(aPeerToPeerContext.PeerToPeerSvcHdle,
UUID_TYPE_128, &uuid16,
251,
CHAR_PROP_NOTIFY,
ATTR_PERMISSION_NONE,
GATT_NOTIFY_ATTRIBUTE_WRITE, /* gattEvtMask */
10, /* encryKeySize */
1, /* isVariable: 1 */
&(aPeerToPeerContext.P2PNotifyServerToClientCharHdle));
.) send data to ble host using function -
aci_gatt_update_char_value(aPeerToPeerContext.PeerToPeerSvcHdle,
aPeerToPeerContext.P2PNotifyServerToClientCharHdle,
0, /* charValOffset */
251, /* charValueLen */
(uint8_t *) pPayload);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.