NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I have been following the STM32WB workshop, however the material seems to not fit to the current FW anymore.I need to read a sensor that is connected via I2C and send the results via BLE.I can get the sensor readings and output them via UART but ...
I am trying to start with stm32wle5j but got stuck with LPTIM irq. I configure it but it always send me Interrupts. I need irq with period 2sec I checked this post, but it didnt help me.https://community.st.com/s/question/0D50X00009XkYEiSAN/huge-repe...
IDE support for BluenRG232 programming ishttps://www.st.com/en/embedded-software/stsw-bluenrg1-dk.htmlWhich other IDE gives support for Blue-nRG232 SOC programming?Can I use Cube ide or IAR platform or TrueStudio for programming the ST Blue nRG232?
HiWe try to enter a dedicated function in out firmware if no BLE stack is installed. Now we have a discussion how this can be done based on the option bytes.Our previously used approach was to check the SBRV value and test it against some expected va...
HiI want to used STM32WB nucleo to program external custom board which has ST controller. I am able program the custom board using STM32L476 nucleo but facing issue with STM32WB nucleo.Please guide me for this.
I have been working through the STM32WB workshop (https://www.st.com/content/st_com/en/support/learning/stm32-education/stm32-moocs/STM32WB_workshop_MOOC.html), which has mostly been excellent. Unfortunately, when I get to workshop 4 (How to modify B...
I've been following the stm32wb workshop using the stm32cubeIDE and i been running in to some difficulties, due to all the documentation being out of date and also unable to run any of the examples on the cubeIDE, has anybody managed to create a proj...
Hi! I flashed my USB dongle with BLE_p2p_client application that I edited on my own. But I can not send more than 3 bytes using aci_gatt_write_without_resp in function tBleStatus Write_Char in the file p2p_client_app.c . Even if I increase CharValLen...
Hi,As we are at the very beginning level of project, and exploring different BLE network topology.1st i would give an overview of the system that we are planning to implement.We have BLE devices / sensors (Appox 100 nos) which are fitted in small com...
Has anyone been successful connecting the BlueNRG-2 SKD (IDB009V1) to either the BlueNRG ST-LINK UTLITIY or IAR 8.40? Both utilizes "CAN'T DETECT". The only tool that seems to detect the SDK is the cumbersome Flash Programmer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.