2020-05-12 5:52 AM
Hello! I can not send more that 3 bytes from client to server using the write characteristic(aci_gatt_write_without_resp) in BLE_p2p_client_app.c . When I change CharValueLetgh to something higher then 3 my board cannot notify anymore. How can I solve this issue?
2020-05-12 5:55 AM
I was able to send more than 3 bytes from client to server. I set aci_gatt_exchange_config(BleApplicationContext.BleApplicationContext_legacy.connectionHandle); in both sides after the connection complete event and set the same CharValueLentgh in both write char's and I was able to send up to 100 bytes!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.