NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, is there any reason why the BL072Z node sometimes loses downlinks?, I am using a single channel gateway working in the 868.1MHz frequency and I have modified the three default channels of the BL072Z node to this frequency, in the uplinks I have n...
Add more details here regarding the question.
I want to find some example of stm32WL.1:in the AN5408 Migrating from STM32L0, STM32L1, STM32L4 Series associated with SX12xxradio, to STM32WLEx microcontrollers, LoRaWAN projects can be found under Projects\NUCLEO-WL55JC\Applications\LoRaWAN,I can n...
I want to do LoRaWAN FUOTA with STM32L4 MCU. So in the implementation it is mentioned the memory has two banks and one bank is used for previous image and one bank for new image. So my query is can we define the size of the bank?
Hello,I developed a PCB for a project using STM32WB55 and after getting it manufactured I am trying to connect it to the computer in order to run the code on it.However, when I connect it to the PC I cannot see the COM port for it. It seemly doesn't ...
Hello, everyone.I have a problem with the board B-L072Z-LRWAN1. I edited the End_Node project of I-CUBE-LRWAN in order to get some packets transmitted by a Decawave device connected to the B-L072-LRWAN1 board.Obviously, I connected the TX-RX pins of ...
Hi, After connecting STM32WB55 eval-kit nucleo board with USB to RS232 cable for debugging the board I see some special(non-readable) characters on debug terminal. I tried few of STM projects but all are giving the same results. These are the se...
I am trying HandsOn4 example for STM32WB55 using firmware version 1.7. The one I am following is based on firmware 1.0. STM32CubeMX with firmware 1.7, has changed the code generation making the original hands on example even more difficult to follow...
I want to do LoRaWAN FUOTA so can i use STM32L1 for that application?In the I-CUBE-LRWAN embedding FUOTA, they only mentioned STM32L4 series MCU.
HiThis is the first time I`m working with STM32 devices apologizes for the beginner questionsI bought an STM32WB55 NucleO Pack (ST part # - NUCLEO-WB55). My intention is to tweak the demo application so that dongle passes same data (readings from int...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.