NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I am trying to design an App for Android and IOS, so I need to use an Bluetooth 4.0 . The problem is that I work with STM32F4 Discovery board, and it won't correctly communicate with the BLE (I think, I'm using a SH-HC-08 and also tried SH-06). W...
I have a STM32WB55CGU6 where I have all my ADC pins used up and im trying to obtain the battery level using a pin which does not have a ADC (PB6) which is branched as shown in the picture attached.This follows the principle where it will charge and d...
Hi, I'm having some difficulties implementing an SPI communication on the STM32WB55 example "Peripheral Lite". I've started from scratch with CubeMX and a i've set up SPI and UART and obtained a working firmware that correctly communicates with an ac...
We have been trying to extend the service over P2P server BLE application . We are trying to add custom template to the existing P2P server project for Bluetooth. When we add custom template through cube Mx generator , the existing line is gettin...
What is the maximum throughput of the STM32WB series actually tested to?As far as I know, nRF82532 central can support 20 links at the same time, how many links can STM32WB central support at the same time?
There is a problem in STM32WB Firmware version in 1.5 and 1.7. In !.5 version Touch sensing is not working and BLE is working fine but In version !.7 Touch sensing is working fine and BLE is not working. Please give me any suitable solution or pleas...
Hi,i have a system with 4 demoboard STM32WB55NUCLEO and 3 STM32WB55DONGLE. One nucleo is a P2P Client, the other 6 are P2P Server. I have modified the examples P2PClient and P2PServer for:direct advertise the client from the 6 serverspair with PASSKE...
Hello , In ProceessTxDone -- receive delay 1 set for 1000 receive delay 2 set for 2000when the MAX_RX_WINDOW set to 3000 the application wont work , which means the second timer event callback wont work e.g ... ...
How with the Sigfox APIs to specify that we want a 20dBm transmission in the RC1?Thanks in advance for your help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.