NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,When generating code from ioc editor with "STM32_WPAN": "BLE" and "BLE Application Type": "Router profile", but "Rounter Mode": "Disabled", the app_conf.h file is generated with error in line 303: enum not completed: /**< Add in that list all t...
I have CubeMX installed and when selecting SMT32WL family I get three BGA devices to select, but when I want to start a project based on these,I get the error: "STM32CubeMX cannot load this Mcu"I have CubeMX 6.0.1 and all packages installed.I would a...
Hi, ST team!My customer uses STM32WB55 in their development and recently he faced with following issue.When the WB into the standby - OK. After out from standby mode all peripherals need repetitive initialization (processes, clocks, memory etc.), but...
Hi all,Could someone help me to clarify about the power consumption of STM32WB55CG, I can't see the difference between 2 series STM32WB55Cx and STM32WB55Rx related to "Low power modes". But in my case, I can put STM32WB55Rx (In Nucleo board) to Stop ...
I have successfully adapted On_Off Zigbee examples for my project. Both router and coordinator works well together. However, the router cannot pair with other coordinator (standard coordinator for Zigbee2mqtt ).I am new for Zigbee. Please give me som...
SBSFU 2.4.0 initializes CPU2 in all cases (for a good reason, locking the AES Key used for decryting the firmware image(s) )When trying to set a HSE tune value (neccessary for proper Bluetooth connectivity) in the application (and also in my loader),...
Hi.I'm wondering about discrepancies in antenna dimensions between AN5129 application note and the actual board - Nucleo MB1335. As you can see the differences are subtle but visible. I'm mostly curious about why the antenna width varies? Widths at d...
Hello! I'm working with an STM32-WB55 nucleo board and trying to put the board into sleep mode. In trying to plan the clocks, I've been working with the *.ioc file to figure out a way to make it work so I know what clock settings to use to put in i...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.