cancel
Showing results for 
Search instead for 
Did you mean: 

How to set up CubeMX for STM32WLE5JCIx or even STM32WLE5CCUx ?

GMaud
Associate II

I have CubeMX installed and when selecting SMT32WL family I get three BGA devices to select, but when I want to start a project based on these,

I get the error: "STM32CubeMX cannot load this Mcu"

I have CubeMX 6.0.1 and all packages installed.

I would also prefer to have the QFN package in the tool, because that is the device I want to use on my boards.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Remi QUINTIN
ST Employee

​Though you can select a WL device, you cannot get any sw supported for it via CubeMX  as it is not officially delivered as of today.

View solution in original post

1 REPLY 1
Remi QUINTIN
ST Employee

​Though you can select a WL device, you cannot get any sw supported for it via CubeMX  as it is not officially delivered as of today.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.