STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Why device using I-Cube-LRWAN software send random data when uplink_counter reach 65535 sent ? Is there any way to modify it ?

Hello Everyone, I'm working with the I-Cube-LRWAN software for LoRa communication in class A device.The device sends data every Tx_Dutycyle period but I have an issue with the software.When using the stack connected to Network such as TTN, I notice t...

How to turn off MAC debugging information in STM32WB

Hello, I am using the STM32WB-P-NUCLEO-WB55 board to do a thread experiment. When I use the serial port assistant to read the messages, I found that many messages that are not on the application layer are displayed.For example, the displayed MAC laye...

0693W000006EHLmQAO.jpg
ZB.1 by Associate II
  • 804 Views
  • 0 replies
  • 0 kudos

Resolved! VBAT Channel Monitoring in the MCU

Datasheet of STM32WB55 mentions that the Maximum voltage that can be given to VBAT is 3.6 V. But, it is also said that there is an internal voltage divider so that voltage to the ADC is 1/3 of the voltage at the VBAT pin So, is it possible to connec...

ASiva.1 by Associate III
  • 3623 Views
  • 3 replies
  • 0 kudos

Resolved! Zigbee stack for STM32WB30 with CubeMX

Hi,I'm looking to create an zigbee endpoint device. I've selected the STM32WB30 for my project and have been configuring in CubeMX. This all goes well.Now I need to flash an wireless stack to the M0, but there is no zigbee stack for the STM32WB30.Doe...

Resolved! Where is the documentation on the Sequencer?

Looks like the Scheduler, SCH_*, have been replaced by the Sequencer, UTIL_SEQ_*. Does anyone know where there is detail description of the Sequencer, along with examples?Thanks,Mark

NPham.11 by Associate
  • 2319 Views
  • 2 replies
  • 0 kudos

STM32WB55 sometimes hangs during BLE Init

I am using the Nucleo STM32WB55 Nucleo Pack to develop BLE applications on the Nucleo board. Every once in a while I have the problem, that the application does not properly start and hangs during BLE Init of the co-processor. This is no problem of m...

MDaub.1 by Associate III
  • 1887 Views
  • 1 replies
  • 0 kudos

no send with the module lora b-l072z-lrwan

hello,I use the B-L072Z-LRWAN Module in Lora, i want test the AT CommandI Join the module AT+JOINAT+NJS=? ==> 0I send AT+SEND=12:hello the response:AT_ERRORI don't understand why?best regardMichel

MArna.19 by Associate
  • 799 Views
  • 0 replies
  • 0 kudos

Resolved! have a problem on linker

I built the project using the STM32CubeExpansion_LRWAN_V1.1.2 example, and I want to use the EEPROM function in LoRa Application.I am trying to declare eeprom related code in a separate file, but the linker cannot import HAL functions.​.\mlm32l07x01\...

DPark.2 by Associate II
  • 3412 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.