NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Dear Members. I'm a beginner and trying to learn and understand how to work with stm32l0 and SH1276. The first task which i set to myself is to reach the absolut minimum power consumption. Watched some tutorials and tried to reach minimum which i me...
Helloi made a customised board using the STM32L476RETx mcu with a lora module : DORJI DRF1262TI opened the project from i-cube-lrwan expansion package with the name SX1262dvk1das USING THE SX1262 AT 868MHz.i updated the PINOUT of my MCU and exclude a...
We have tried usingNVIC_SystemReset();but it seems it only resets the M4 core and not the M0+ responsible for Bluetooth communication. It would be really appreciable if someone could guide us towards identifying the cause behind this behavior, and ho...
It appears that v1.10 of the Thread FTD binary does not work properly. When a command is sent (line 4 below), the code stalls in an infinite loop, waiting for an ACK from the M0 processor.static void APP_THREAD_DeviceConfig(void) { otError error; ...
The printed message is:▒▒RT ▒▒▒n▒▒ E▒amp▒▒ ▒▒▒a▒g▒▒ ▒h▒ C ▒▒b▒a▒y p▒▒n▒▒ ▒un▒▒▒▒n ▒▒ ▒h▒ ▒▒RT▒Insteadprintf("UART Printf Example: retarget the C library printf function to the UART\n\r");
Hi,i have 2 boards (client and server) with STM32WB that communicates through BLE messages. Right now, at every reboot/disconnection i am redoing the pairing, but it is really slow.In order to reduce the whole connection time, i am trying to use the ...
i want to initialize pin A9 & A10 in BL072ZLrWAN1board of STas a external interrupt pin. ICubeLrwan package not integrate with cubeMX so i am confuse about how to initialize the pin and call the interrupt and write its callback function.
Hi,We are currently working on an usb composite library but some old FLASH ghosts reappeared.When sending data through a cdc flash started to fail some erase/program.We decided to upgrade our Wireless stack to latest (1.10.0) from our current 1.6.0 (...
Greetings,My application for the STM32WB uses the BLE full stack from v1.8 of the Cube. I just noticed that there is a v1.10. I plan to test this as well, just in case this has been fixed.The cube has code to manipulate the SRAM2 parity options, but ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.