STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

How to use P-NUCLEO-WB55 USB Dongle as a USB BLE Radio?

Is there a firmware package I can use with the P-NUCLEO-WB55 USB Dongle so that I can use that dongle as a USB BLE Radio? I want to be able to develop a BLE device (Nucleo board) as a bluetooth device but my Windows PC doesn't have a Bluetooth radio ...

DK.6 by Associate II
  • 896 Views
  • 0 replies
  • 0 kudos

HOW TO USE COMP1 in STM32 -LRWAN1 board

I used STM32-B-L072Z-LRWAN1 board and want to used COMP 1 and COMP2 in my project.to used COMP1 as per data sheet PA1 can be used as inputbut on STM32 LORA board its not incorporated.I want to know where PA1 is used ,any doc is useful.Can I used this...

0693W000006FXsoQAG.png

With the "STM32 LoRa® Expansion Package" is it possible to set the RTC time after initialization of the Lora stack.

I would like to be able to set the time from the LoRa network. So when I receive the time I make a HAL_RTC_SetTime with the information collected, but then my program freezes. Do I have to stop the Lora layer, timers beforehand?Thank you in advance f...

LeJiBXL by Associate
  • 1227 Views
  • 1 replies
  • 0 kudos

STM32WB USB bootloader

HiI`m having some issues with programming p-nucleo usb dongle board with USB DFu mode.The way I understand is ,there is an internal system bootloader inside STM32WB which supports USB Firmware DownloadIf I can jump to bootloader from my application ...

TGUCL.1 by Associate III
  • 1027 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.