cancel
Showing results for 
Search instead for 
Did you mean: 

I-CUBE-LRWAN don't work on custom board: PHY txTimeOut ERROR

SHATE.1
Associate III

Hello

i made a customised board using the STM32L476RETx mcu with a lora module : DORJI DRF1262T

I opened the project from i-cube-lrwan expansion package with the name SX1262dvk1das USING THE SX1262 AT 868MHz.

i updated the PINOUT of my MCU and exclude all unnecessary driver and board sensor not used.

when i compile, everything is OK with error and warnings

i program my board. the program run but in 4s112ms the program is bloqued and the message in the UART of " 4s112 ms PHY txTimeOut " is printed and everything is stopped.

SPI pin and CS and DIO1 are well connected and in the beginningof the run, i see a signal on this protocole. the board well worked in ping pong mode with another board

Please help

Thank you

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

https://community.st.com/s/question/0D53W00000JNMqBSAX/lora-sx1262-tx-timeout

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.