STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! How to increase LPAWUR range

Hello :) I am developing an application using a pair of NUCLEO-WL33CC1. I am testing the LPAWUR, using the LPAWUR_WakeupRadio_Rx and MRSUBG_WakeupRadio_Tx examples as a starting point. The examples work fine, but the range is very short, only about 0...

angus123 by Associate III
  • 1582 Views
  • 7 replies
  • 5 kudos

Resolved! STM32WB5MMG read characterisitc

Hi, I want to make a simple application with an STM32WB5MMG that exposes a characteristic which I can read. I created the service and the characteristic, and I enabled the CHAR_PROP_READ property. In custom_app.c, I then use Custom_STM_App_Update_Cha...

How to get XX_SCAN_REQUEST_XX event

ST ,I am working on getting the scan request event ob the full stack.After looking at these posts : https://community.st.com/t5/stm32-mcus-wireless/ble-how-can-i-get-a-scan-request-event/td-p/221485https://community.st.com/t5/stm32-mcus-wireless/ble-...

DS4_0-1753722639206.png
DS.4 by Senior II
  • 860 Views
  • 4 replies
  • 0 kudos

LoRaWAN: Switch from Class C to A

Split from L072Z LRWAN1: Switch from Class C to AI also encountered the problem of CLASSC conversion failure. Could you please tell me if you have any solutions at present

dannyhui by Associate II
  • 590 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WBA65RI FlashManager stuck writing to FLASH

Hello,I am working to incorporate BLE bonding into our project, and have run into a tricky issue where the Flash Manager gets stuck trying to write a key to flash. I've enabled the Flash Manager and SNVMA_NVM modules in the IOC file:I'm currently usi...

JFisherLegato_0-1758046734786.png

Resolved! Programming NUCLEOWB55RG board with another board

I want to program a NUCLEOWB55RG board with another identical NUCLEOWB55RG. The reason is the other NUCLEO board is placed on a PCB and is powered externally, so i cannot connect USB to it. Do I just remove the JP1 jumper and connect the SWD pins (SW...

Resolved! STM32WL30 change USART baud rate

Hello everyone,I'm working with the STM32WL30 and I'm trying to change the baud rate of the USART peripheral. However, I'm encountering some issues when I change the baud rate.The function I wrote for changing the baud rate looks like this:void chang...

PhilippR by Associate II
  • 966 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.