2025-09-16 11:20 AM
Hello,
I am working to incorporate BLE bonding into our project, and have run into a tricky issue where the Flash Manager gets stuck trying to write a key to flash. I've enabled the Flash Manager and SNVMA_NVM modules in the IOC file:
I'm currently using RTT Viewer for logging, and this is the output I see:
00> FM_WindowAllowed_Callback
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
00> HAL_FLASH_Program: Address: 0x081FE000, DataAddress: 0x2002F610 (status: 0x00000000)
00> FM_BackgroundProcess - Flash operation not complete yet, request a new time window
00> FM_WindowAllowed_Callback
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
00> HAL_FLASH_Program: Address: 0x081FE000, DataAddress: 0x2002F610 (status: 0x00020000)
00> FM_BackgroundProcess - Flash operation not complete yet, request a new time window
00> FM_WindowAllowed_Callback
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
00> HAL_FLASH_Program: Address: 0x081FE000, DataAddress: 0x2002F610 (status: 0x00020000)
00> FM_BackgroundProcess - Flash operation not complete yet, request a new time window
00> FM_WindowAllowed_Callback
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
00> HAL_FLASH_Program: Address: 0x081FE000, DataAddress: 0x2002F610 (status: 0x00020000)
00> FM_BackgroundProcess - Flash operation not complete yet, request a new time window
00> FM_WindowAllowed_Callback
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
00> HAL_FLASH_Program: Address: 0x081FE000, DataAddress: 0x2002F610 (status: 0x00020000)
00> FM_BackgroundProcess - Flash operation not complete yet, request a new time window
00> FM_WindowAllowed_Callback
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
00> FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
00> HAL_FLASH_Program: Address: 0x081FE000, DataAddress: 0x2002F610 (status: 0x00020000)
(continues...)
Note: I've added the logging line in HAL_FLASH_Program. As you can see, it is the WDW bit that appears to be stuck, which to me indicates that the write did not happen fully. When I pause in the debugger and step through the code, the write works fine. However, it is failing when I let it run as a program.
I'm happy to share our IOC file directly, if that's useful.
Thank you,
Jonathan
Solved! Go to Solution.
2025-09-16 1:25 PM
This is interesting: it appears that using a JLink to load the board uses the FLASH registers, and leaves them in a non-reset state. If I add this: CLEAR_BIT((*reg_cr), FLASH_NSCR1_BWR); to the FLASH_Program_QuadWord() function, I am able to run as expected.
2025-09-16 12:03 PM
An interesting piece of information is that despite FLASH_Program_Burst() never being called, the FLASH_NSCR1.BWR bit is set, indicating burst write. Digging into this further!
2025-09-16 1:25 PM
This is interesting: it appears that using a JLink to load the board uses the FLASH registers, and leaves them in a non-reset state. If I add this: CLEAR_BIT((*reg_cr), FLASH_NSCR1_BWR); to the FLASH_Program_QuadWord() function, I am able to run as expected.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.