2021-02-23 7:26 AM
Sorry ST guys but the UART HAL and LL_HAL ist a total fail!
I developing over 15 years all kind of serial communication with linux and different microcontrollers. Now I regret my desistion to use the STM32WB MCU.
I'm trying over two weeks the get a stable UART communication running with different data length (5 to 50 bytes). All tries with DMA or Interrupt are failed. All this ST HAL examples are not realy usefull and if I search for some input I can read a lot and I mean a loooot of similar problem at the forums....
Now I have to think about to went awai from this MCU or I have to write my own working HAL from scratch.
It seams the marketing did a good job but the rest ???? I dont know....
A unhappy user....
2021-02-23 10:30 AM
Sorry to hear that. Not sure if marketing is listening because most people here are community developers. Maybe you want to share stripped down code here, showing your issues.
KnarfB
2021-02-23 12:35 PM
Okay, and have you tried the good old readin the manual and proceed accordingly, step by step?
Polled UART is hardly a rocket science and interior is not much harder. DMA is next step.
JW
2021-02-24 10:08 AM
STM32 HAL USART reality:
Expecting such a broken bloatware to perform reliably is illogical. Typically the strategy of HAL developers and users is to ignore the bugs and pretend they do not exist. In case of USART for something sane look here:
https://github.com/MaJerle/stm32-usart-uart-dma-rx-tx
That said, the STM32 hardware is mostly pretty nice and decent. Therefore write your own sane software and... the sky is the limit.
2021-02-25 12:34 AM
I started from zero with a new STM32CubeMX and STM32CubeIDE project including the latest HAL librarys. I use the Nucleo dev board and create a UART setup with interrupts, thats all.
static void MX_USART1_UART_Init(void)
{
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_8;
huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
{
Error_Handler();
}
}I can receive fixed data lenght with 5 bytes:
HAL_UART_Receive_IT(&huart1, (uint8_t *)Rx_Buffer, 5);The MCU is sending the answer with:
HAL_UART_Transmit_IT(&huart1, buffer, bufsize);BUT the data are NOT right in any way:
If I send the exact same buffer content with: HAL_UART_Transmit(&huart1, buffer, bufsize, 20); the data are transmitted right!
Now thats the big question why HAL_UART_Transmit_IT() can not send the data right??? There is nothing else running at this code, it just receive and sends some data. How the MCU should work savely in combination with some real working code if the HAL cannot do the simple serial job?? In this case I can not trust the HAL library.
2021-02-25 12:36 AM
Welcome to the 21 century, but polling was maybe ok in the 80ies. Polling it no rocket science thats right, but if you want to use a high end MCU/CPU thats the totaly wrong way....
Why put ST this effort into examples and libraries which are not working properly. A stable serial communication should be/is the basic for all MCU...
2021-02-25 12:44 AM
Thanks Piranha for your clear words and it confirms my assumption. I will check out the USART example you posted. The documentation looks promising to get a save an good solution...
2021-02-25 3:43 AM
Hi @STUser21 ,
I am interested to get your complete project to reproduce the issue on my side. So could you please share your main.c & .ioc files?
How you declare buffer variable and how you are calling HAL_UART_Transmit_IT may have impact.
Thanks.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-03-24 6:16 AM
Dear @STUser21
As mentioned by @Amel NASRI , would it be possible for you to share your project, to investigate your issue ?
Thanks a lot.
Guenael
2021-03-25 8:45 AM
Hello, the project is now on hold because of some other priorities. I will be back if there is some time left...
Thanks for your interest.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.