NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello, I have already received package STM32 Nucleo Pack - LoRa HF band sensor and gateway - containing sensor board with USI chip.Today I attended pre-workshop with Bartosz Boryna and it looks like that the board with USI is useless now, I need some...
Hi, Is there any way to read register data in STM32WL? Since it uses SX1262 chip, I want to read register data using the register address. Since STM32WL does not have SPI support, can anyone please suggest how to read register data using STM32WL? Fo...
Hi,I need to advertise free data, as I understand it is located in manufacturer data section.When I advertise only the manufacturer data, with aci_gap_update_adv_data function, I can see with Application BLE Scanner, the data, as raw data.But when I ...
HiI couldn't find a specific definition of the total length that I can advertise.On one place I saw 37 bytes, on another place only 25 bytes.Can someone tell me, how many bytes can I advertise? Thanks,Lior
I tried flashing PWR_STANDBY_RTC and PWR_EnterStandbyMode examples both has sleep current of 590uA. How do i get the datasheet value of 600nA standby current or atleast something less than 10uA.
I have started to go through the course pre-requisites and am familiarising myself with the kit and feeling much more confident, particularly as I have the gateway setup on TTN an seeing the L073RZ dev board ping in. I am still going through the prer...
My project requires a RS-232 cable with TX inverted to connect the PC with CubeProgrammer CLI to STM32WB55. In application, I am able to configure the UART with "UART_ADVFEATURE_TXINVERT_INIT", and the STM32WB55 transmission works fine through the RS...
Hi,Im using STM32WB55 USB dongle board. I want to send data from the dongle board to PC using USB pheriperal. i used the command CDC_Transmit() to send data and I visualized the recieved data using realterm in PC . It was working. But I want to...
Hi,I am new to the STM32WB range. I need to use the 1MB flash version in a project, But I am struggling a bit to understand the flash layout.I read that the first 6 Sectors are to be used my the OTA application. It seems like settings should go direc...
Hello to everyone,I have two B-L072Z-LRWAN1 kit. Trying for measure best distance i can reach. I am using Ping-Pong example and change some variables such as LORA_SPREADING_FACTOR, LORA_BANDWIDTH, LORA_CODINGRATE, LORA_PREAMBLE_LENGTH etc. Until now,...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.