NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi everybody, yesterday I was working with my Nucleo68 board of the P-NUCLEO-WB55 pack as always, however something go wrong after to did this:I modified the WWDGSW and IWDGSW option bytes with STM32CubeProgrammer (from checked to unchecked, and appl...
I am using the STM32WB55 ADC with the internal reference VREFBUF set to 2V5. To save power consumption, the application disables VREFBUF before going to sleep and enables it just after waking up. The problem is that I am making measurements with the ...
If I use STM32WL as RF tranciver and using the (G)FSK modultion or other modulation with multiple users, Will STM32WL asigne a carrier frequency automatically for each user to achieve the FDMA as PMR/DMR system in walkie talkie?
Hi, I am running the BLE_DataThroughput example for the STM32WB55 with two boards as described in the documentation- one set as a client, one as a server. I have connected the client board to a desktop PC via UART, and I am monitoring the output with...
Hi there, I'd like to know if the USB port on the stm32wl55 can be used as a virtual com port and if so, how to achieve that.
Hello,I use a STM32WB55RGV7 microcontroller. Doing the hardware layout I'm confused about the antenna filter: - I can't get the band pass filter LFB182G45CGFD436 in small quantities, which is used in the P-Nucleo-WB55 - the low pass filter LFL212G45T...
I have a custom hardware with an STM32WLE5C8Ux and I want to add functionality to it step by step. I'm using CubeMx to generate a project with success ,toggeling a GPIO works. I have not initalized external TCXO or LSE, they are populated but I want ...
Hi!I can't find the WLCSP59-Package at distributors like digi-key, mouser etc. It doesn't seem to be available. Does anyone know why?Is this a matter of time (not in mass production yet) or a matter of volume (only sold to specific customers)?If the ...
I read some contradictory information and I am not sure what is true. According to the document https://www.google.com/url?sa=t&rct=j&q=&esrc=s&source=web&cd=&ved=2ahUKEwjX3NCZvoDwAhVIY8AKHe2zCrkQFjAAegQICBAD&url=https%3A%2F%2Fwww.st.com%2Fcontent%2F...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.