NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I bought NUCLEO-WL5JC2 Low Band (As NUCLEO-WL5JC1 were not in stock)Is it possible to turn them into High Band by changing some passive components ? So I can use them in 868Mhz instead of 433Mhz Thanks
I am trying to do the example "HandsOn_2" from STM32WB_workshop. Executes commands as described. The only difference is I use STM32Cube_FW_WB_V1.3.0 instead of STM32Cube_FW_WB_V1.0.0.STM32Cubex does not copy the scheduler.c, scheduler.h files to the ...
I want to reset and reinitialize only CPU2 (M0 +) of STM32WB I used to ask a question in "Data reception stops at Mac_802_15_4_FFD in the sample code."Even now, this matter has not been resolved.At the end, it was said that RFD was used, but since I ...
Environment:MacOS 10.14.6STM32CubeIDE 1.6.1STM32WB SDK 1.11.0Starting with a clean install of Cube, SDK, empty workspace. Importing p2p_Server project (from the initial splash screen->Import STM32 sample app), the build fails with (among other):/Use...
In the pack FP-AUD-BVLINKWB1, BLE audio streaming example provided with Opus codec, will you be also providing similar example using new LE audio standard with LC3 codec?
Namaste from India.I am working on STM32WB Nucleo board for BLE functionality as per the tutorial available: https://www.youtube.com/watch?v=zNfIGh30kSsI have copied the codes from workshop snippets provided by ST. When I press the LED on the ST BLE ...
Hello,function "aci_gap_delete_ad_type" returns value "0x1F". This value is not defined in file "ble_defs.h" at lines 192ff like other return values ("BLE_STATUS_SUCCESS" etc.)Do you confirm that the meaning of "0x1F" is "AD_TYPE not found" ?Can you ...
I need to program the chip use JTAG or SWD, But now i could just read the jtag id. i could not access the flash. so is there special document for how to access the flash using JTAG or SWD interface.
I am going to download the ble stack to stm32wb55 using the program. On P-NUCLEO-WB-55, it was downloaded properly, but I tried the same thing on my custom board, but it failed.This is the log we did on NUCLEO-WB55 below.Deleting previous wireless st...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.