NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi , I was using LoRaWAN_AT_Slave example code for NUCLEO-WL55JC1 Board on STMCUBEIDE .AT command response was OK but , the configured values are not getting stored into flash (upon reset getting the default values)..CONTEXT_MANAGEMENT_ENABLED and M...
Hi, I would like to store the data acquired from external sensor to my AWS cloud, is there any app that can help with this ? There is option of "Cloud Logging" in "ST BLE sensor" smartphone app , is this option meets my requirements ?Thank you in adv...
I am using the Nucleo WB55 Development Board, how do I set up the (Programmable voltage detector) PVD and get it to work?
I would like to look at the register to see which values are stored inside that register. Then I would like to use that number to do operations.
When starting connectable undirected advertising mode by calling "aci_gap_set_discoverable(...)" it turns out that the advertiser sends AD with "Flags" type (0x01) and "TX power level" type (0x0A). As a restriction of the application, I need to remov...
Does stm32wb support homekit?
Hi, the timers of my STM32WB55x aren't working exactly as I anticipated.Symptoms: By conventional wisdom that I accumulated when using other MCUs under different brands, if the CNT is modified to a different value, the counter should keep counting fr...
Dear ST community, I have 2 Nucleo WL55 highband boards and I suspect that there has been a mislabelling of the device. As I am aware of, only the D-04 version of this board is sold. However, my board has several pins that do not correspond to the on...
I'm trying to get started using the STM32WLE5-series chip, and I'm really struggling to figure out how to get the `AT` firmware example going. I see it in the SDK package, but it's only for the STM32WL5-series (dual-core) chips. I see this setting ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.