STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB55 USB dongle not responding to CubeMonitor-RF

I want to connect to the WB55 USB Dongle with CubeMonitor-RF to scan for my BLE peripherals.I followed the connection guide and flashed the BLE_TransparentModeVCP firmware to the dongle. I also installed the VCP driver under windows. The dongle appea...

0693W00000AOfLmQAL.jpg
A.D. by Senior
  • 2126 Views
  • 4 replies
  • 1 kudos

Resolved! HSE optimization

Hi,Using the P NUCLEO WB 55 with STM32WB .Encountered with below code, regarding HSE tuning, in workshop tutorial. A reference was given to An5024.This code does not exist in my example project, BLE Heart Rate RTOS, generated with STM32Cube 6.2.0 , F...

0693W00000APKqHQAX.png
DS.4 by Senior II
  • 1788 Views
  • 1 replies
  • 0 kudos

STM32WLE5C8 : region `FLASH' overflowed by *** bytes0

Hi everyone :)I'm at the first steps of building a Lora application with STM32WLE5C8 MCU. While using CubeMX to generate the code, and after defining the pinout of the chip, connectivity, and LORWAN in middleware, I opened the project in CudeIDE and ...

Iaomari by Associate II
  • 4010 Views
  • 5 replies
  • 0 kudos

GMSK RX/TX

In this doc searching for the keyword MSK I come across the following:"MSK and GMSK RX/TX with BR from 1.2 to 300 Kbit/s and TX only with BR from 0.1 to 1.2 Kbit/s""The (G)MSK and BPSK modems only supports transmission""The FSK modem with a bit rate ...

MCarl.7 by Associate II
  • 1642 Views
  • 1 replies
  • 0 kudos

How do I reconnect end-device routing with Zigbee 3.0?

Hello All; I use an example code "Zigbee_OnOff_Client_Router" for Nucleo-STM32WB and "Zigbee_OnOff_Server_Coord" for Dongle-STM32WB when my coordinator lose then come back. My rounter can't send any message to coordinator. Could you please advice ...

Gz by Senior
  • 873 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.