NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
HiMe and my team designed a custom PCB containing a STM32wb55cc and needed it to be connected with BLE with an application made by ourself. Unfortunately, even if ou board is functionning pretty well with STM apps like with STM32 BLE toolbox for Andr...
Bluetooth Mesh Rapid Prototyping workshop using the STM32WB5MM-DK
Hi,I am using a STM32WB5MMG module and want to use FreeRTOS in combination with BLE.For ease of programming I am using CubeMX to set everything up. My goal is to have BLE up and running to be able to connect it to a Client. FreeRTOS is being used to ...
I followed the series of video "STM32WB Getting Started" with my P-Nucleo-WB55 board. During the 5th video "Heart Rate Monitor", I flashed the BLE_HeartRate project into my board and since this I have this message :"Target no device foundError in ini...
I just loaded version 2 of the AT slave firmware on my B-L072Z-LRWAN1 discovery kit and noticed that the current measured over JP3 which heads to the MCU oscillates between 2.5mA and 2.9 uA every 50 milliseconds. When I flashed the device with ol...
Good Day.I have created a board and some program easily through SWD port and some struggle. The error i am getting In STM32CubeProgrammer is:---------------------------------------------08:35:51:413 : Reconnected !08:35:51:413 : Success with Time ela...
i'm using P-NUCLEO-WB55i try to update bootloader using stm32wb wiress stack updater.I saw the link below and set up the hardware for bootloader.https://visualgdb.com/tools/STM32WBUpdater/connecting/When I connected the usb, I could see DFU in FS Mod...
In testing my LoRa design at 868 MHz on the STM32WL with a digitally compensated TCXO I witness a significant jump in frequency when (what I assume is) a micro-jump of the TCXO occurs. The specification rate this as maximum 300ppb which equates to w...
Hello,I build a network that have some coordinators(FFD) and few nodes(RFD) by using;Dev-kit: STM32WB55 NucleoSW: Mac_802_15_4_FFD (from STM32Cube_FW_WB_1.11.0)I want to send a message that will be received by all nodes and all coordinators nearby. ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.