2021-05-21 3:19 AM
2021-05-21 4:04 AM
Which part specifically?
Does it work in point-to-point mode with test firmware?
Does it work if you use a regular TCXO?
How are you controlling the TCXO compensation?
2021-05-21 5:00 AM
Well, this looks like a normal TCXO (3225 package); the thermal compensation is integrated , but apparently this compensation circuit can be analog or digital. Analog is hard to find these days because of shortage in raw material (AKM), digital is probably cheaper, but works with (tiny) discrete compensation steps.
The device works perfectly with a TCXO featuring analog compensation and also using an external clock generator.
Example of the TCXO with digital compensation: STC32K30P48-32.000M (https://suntsu.com/wp-content/uploads/2021/01/STC32K-Series.pdf)
2021-05-21 7:43 AM
Ok, Have you looked at the clock signal with a modulation domain analyzer?
2021-05-25 4:13 AM
No, we logged the clocksignal using a spectrum analyser (zero span, 30Hz res. BW) and see discrete steps; one of these 'steps' within an active transmission leads to CRC errors on the receiving side.
We're quite sure aboute cause & effect; would be good to hear if someone experienced the same or can explain exactly why this type of TCXO is incompatible with the LoRa Xcvr-HW.
2021-05-25 4:16 AM
Insufficent supply decoupling/strength?
2021-05-25 4:18 AM
Don't think so: we tried external (clean) supply for TCXO and clockbuffer for 32MHz to avoid problems with clock loading, but none of these changed the behavior.
2021-05-25 5:23 AM
What frequency step did you observe?
Is the board exposed to changing environment conditions, e.g. wind? Does the board have changing thermal sources, so that the TXCO sees rapid temperature changes? In case of wind or other turbulance, try some thermal isolation around the TXCO. For board thermal siources, keep the TXCO far away from these sourcessources of heat on your board and perhaps isolate by milling.
2021-05-25 7:17 AM
The exact magnitude of the step has not been identified (we don't have the equipment available), but the TCXO is spec'ed for 2ppm and I'm sure it operates within spec so it's probably a sub-ppm shift.
All measurements took place in a lab-environment; the TCXO is positioned next to the xcvr, which means the compensation of the TCXO is caused by self-heating (PA).
Indeed, milling could reduce this effect, but it will not guarantee error-free operation in the field.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.