2021-06-02 9:50 AM
Hi,
I am using a STM32WB5MMG module and want to use FreeRTOS in combination with BLE.
For ease of programming I am using CubeMX to set everything up.
My goal is to have BLE up and running to be able to connect it to a Client. FreeRTOS is being used to communicate with a LTE Modem and several sensors.
Currently I am stuck on getting the device to boot up properly.
Without the stm_wpan part enabled in CubeMX my code is working fine, but as soon as I enable it, the code gets stuck after power up.
I am basically using the BLE_HeartRateFreeRTOS example but added my code to the default task
Really appreciate any help !!
Thanks in advance
/* USER CODE END 4 */
/* USER CODE BEGIN Header_StartDefaultTask */
/**
* @brief Function implementing the defaultTask thread.
* @param argument: Not used
* @retval None
*/
/* USER CODE END Header_StartDefaultTask */
void StartDefaultTask(void *argument)
{
/* USER CODE BEGIN 5 */
app();
/* Infinite loop */
for(;;)
{
osDelay(1);
}
/* USER CODE END 5 */
}/* USER CODE BEGIN Header */
/**
******************************************************************************
* File Name : app_entry.c
* Description : Entry application source file for STM32WPAN Middleware
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2021 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under Ultimate Liberty license
* SLA0044, the "License"; You may not use this file except in compliance with
* the License. You may obtain a copy of the License at:
* www.st.com/SLA0044
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "app_common.h"
#include "main.h"
#include "app_entry.h"
#include "app_ble.h"
#include "ble.h"
#include "tl.h"
#include "cmsis_os.h"
#include "shci_tl.h"
#include "stm32_lpm.h"
#include "app_debug.h"
/* Private includes -----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
extern RTC_HandleTypeDef hrtc;
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private defines -----------------------------------------------------------*/
#define POOL_SIZE (CFG_TLBLE_EVT_QUEUE_LENGTH*4U*DIVC(( sizeof(TL_PacketHeader_t) + TL_BLE_EVENT_FRAME_SIZE ), 4U))
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macros ------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
PLACE_IN_SECTION("MB_MEM2") ALIGN(4) static uint8_t EvtPool[POOL_SIZE];
PLACE_IN_SECTION("MB_MEM2") ALIGN(4) static TL_CmdPacket_t SystemCmdBuffer;
PLACE_IN_SECTION("MB_MEM2") ALIGN(4) static uint8_t SystemSpareEvtBuffer[sizeof(TL_PacketHeader_t) + TL_EVT_HDR_SIZE + 255U];
PLACE_IN_SECTION("MB_MEM2") ALIGN(4) static uint8_t BleSpareEvtBuffer[sizeof(TL_PacketHeader_t) + TL_EVT_HDR_SIZE + 255];
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Global variables ----------------------------------------------------------*/
osMutexId_t MtxShciId;
osSemaphoreId_t SemShciId;
osThreadId_t ShciUserEvtProcessId;
const osThreadAttr_t ShciUserEvtProcess_attr = {
.name = CFG_SHCI_USER_EVT_PROCESS_NAME,
.attr_bits = CFG_SHCI_USER_EVT_PROCESS_ATTR_BITS,
.cb_mem = CFG_SHCI_USER_EVT_PROCESS_CB_MEM,
.cb_size = CFG_SHCI_USER_EVT_PROCESS_CB_SIZE,
.stack_mem = CFG_SHCI_USER_EVT_PROCESS_STACK_MEM,
.priority = CFG_SHCI_USER_EVT_PROCESS_PRIORITY,
.stack_size = CFG_SHCI_USER_EVT_PROCESS_STACK_SIZE
};
/* Private functions prototypes-----------------------------------------------*/
static void ShciUserEvtProcess(void *argument);
static void SystemPower_Config( void );
static void appe_Tl_Init( void );
static void APPE_SysStatusNot( SHCI_TL_CmdStatus_t status );
static void APPE_SysUserEvtRx( void * pPayload );
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Functions Definition ------------------------------------------------------*/
void APPE_Init( void )
{
SystemPower_Config(); /**< Configure the system Power Mode */
HW_TS_Init(hw_ts_InitMode_Full, &hrtc); /**< Initialize the TimerServer */
/* USER CODE BEGIN APPE_Init_1 */
/**
* The Standby mode should not be entered before the initialization is over
* The default state of the Low Power Manager is to allow the Standby Mode so an request is needed here
*/
UTIL_LPM_SetOffMode(1 << CFG_LPM_APP, UTIL_LPM_DISABLE);
/* USER CODE END APPE_Init_1 */
appe_Tl_Init(); /* Initialize all transport layers */
/**
* From now, the application is waiting for the ready event ( VS_HCI_C2_Ready )
* received on the system channel before starting the Stack
* This system event is received with APPE_SysUserEvtRx()
*/
/* USER CODE BEGIN APPE_Init_2 */
/* USER CODE END APPE_Init_2 */
return;
}
/* USER CODE BEGIN FD */
/* USER CODE END FD */
/*************************************************************
*
* LOCAL FUNCTIONS
*
*************************************************************/
/**
* @brief Configure the system for power optimization
*
* @note This API configures the system to be ready for low power mode
*
* @param None
* @retval None
*/
static void SystemPower_Config(void)
{
/**
* Select HSI as system clock source after Wake Up from Stop mode
*/
LL_RCC_SetClkAfterWakeFromStop(LL_RCC_STOP_WAKEUPCLOCK_HSI);
/* Initialize low power manager */
UTIL_LPM_Init();
/* Initialize the CPU2 reset value before starting CPU2 with C2BOOT */
LL_C2_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN);
#if (CFG_USB_INTERFACE_ENABLE != 0)
/**
* Enable USB power
*/
HAL_PWREx_EnableVddUSB();
#endif
return;
}
static void appe_Tl_Init( void )
{
TL_MM_Config_t tl_mm_config;
SHCI_TL_HciInitConf_t SHci_Tl_Init_Conf;
/**< Reference table initialization */
TL_Init();
MtxShciId = osMutexNew( NULL );
SemShciId = osSemaphoreNew( 1, 0, NULL ); /*< Create the semaphore and make it busy at initialization */
/** FreeRTOS system task creation */
ShciUserEvtProcessId = osThreadNew(ShciUserEvtProcess, NULL, &ShciUserEvtProcess_attr);
/**< System channel initialization */
SHci_Tl_Init_Conf.p_cmdbuffer = (uint8_t*)&SystemCmdBuffer;
SHci_Tl_Init_Conf.StatusNotCallBack = APPE_SysStatusNot;
shci_init(APPE_SysUserEvtRx, (void*) &SHci_Tl_Init_Conf);
/**< Memory Manager channel initialization */
tl_mm_config.p_BleSpareEvtBuffer = BleSpareEvtBuffer;
tl_mm_config.p_SystemSpareEvtBuffer = SystemSpareEvtBuffer;
tl_mm_config.p_AsynchEvtPool = EvtPool;
tl_mm_config.AsynchEvtPoolSize = POOL_SIZE;
TL_MM_Init( &tl_mm_config );
TL_Enable();
return;
}
static void APPE_SysStatusNot( SHCI_TL_CmdStatus_t status )
{
switch (status)
{
case SHCI_TL_CmdBusy:
osMutexAcquire( MtxShciId, osWaitForever );
break;
case SHCI_TL_CmdAvailable:
osMutexRelease( MtxShciId );
break;
default:
break;
}
return;
}
/**
* The type of the payload for a system user event is tSHCI_UserEvtRxParam
* When the system event is both :
* - a ready event (subevtcode = SHCI_SUB_EVT_CODE_READY)
* - reported by the FUS (sysevt_ready_rsp == FUS_FW_RUNNING)
* The buffer shall not be released
* ( eg ((tSHCI_UserEvtRxParam*)pPayload)->status shall be set to SHCI_TL_UserEventFlow_Disable )
* When the status is not filled, the buffer is released by default
*/
static void APPE_SysUserEvtRx( void * pPayload )
{
UNUSED(pPayload);
/* Traces channel initialization */
APPD_EnableCPU2( );
APP_BLE_Init( );
UTIL_LPM_SetOffMode(1U << CFG_LPM_APP, UTIL_LPM_ENABLE);
return;
}
/*************************************************************
*
* FREERTOS WRAPPER FUNCTIONS
*
*************************************************************/
static void ShciUserEvtProcess(void *argument)
{
UNUSED(argument);
for(;;)
{
/* USER CODE BEGIN SHCI_USER_EVT_PROCESS_1 */
/* USER CODE END SHCI_USER_EVT_PROCESS_1 */
osThreadFlagsWait(1, osFlagsWaitAny, osWaitForever);
shci_user_evt_proc();
/* USER CODE BEGIN SHCI_USER_EVT_PROCESS_2 */
/* USER CODE END SHCI_USER_EVT_PROCESS_2 */
}
}
/* USER CODE BEGIN FD_LOCAL_FUNCTIONS */
/* USER CODE END FD_LOCAL_FUNCTIONS */
/*************************************************************
*
* WRAP FUNCTIONS
*
*************************************************************/
void shci_notify_asynch_evt(void* pdata)
{
UNUSED(pdata);
osThreadFlagsSet( ShciUserEvtProcessId, 1 );
return;
}
void shci_cmd_resp_release(uint32_t flag)
{
UNUSED(flag);
osSemaphoreRelease( SemShciId );
return;
}
void shci_cmd_resp_wait(uint32_t timeout)
{
UNUSED(timeout);
osSemaphoreAcquire( SemShciId, osWaitForever );
return;
}
/* USER CODE BEGIN FD_WRAP_FUNCTIONS */
/* USER CODE END FD_WRAP_FUNCTIONS */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.