NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,I am a bit confused on the lora STM32WL sequence protocol system, I want my device to sleep and wakeup according to the periodic values I want. I have made my own sleep function (stop 2 mode & radio sleep) with wake up triggered using RTC (in seco...
Hi,I'm hoping that someone can help me implement a Channel Activity Detection (CAD) check on a TX channel before transmitting a message, as to implement a kind of CSMA version of LoRa. Basically I would like to know where CAD is carried out in the Lo...
A new version 2.7.1 is released. Fixed sniffer issues :Remove extra FCS bytes in frames.Stop then start capture with no frame raised an error.Enjoy !
I tried to run BLE Blood pressure example on my STM32WB board.I was able to connect to BLE and see the screen as attached. But the example stated that value updates every 4 secs. What am I doing wrong here? Do I need to make any changes in program? I...
I am moving our BLE development from Zephyr 2.5.0 to 2.6.0. The st_ble_sensor sample included in the Zephyr 2.5.0 tree compiles and runs successfully with the nucleo_wb55rg eval board, but does not work when I attempt the sam from the Zephyr 2.6.0 tr...
Development board: L072CZ-LRWAN boardDevelopment Environment: KEIL (Free License)HelloWe are currently developing LoRaWAN's end device.Before connecting JP9 1-2 to control TCXO,I tried to check if the output is coming from PA12, but only the voltage ...
개발 보드 : L072CZ-LRWAN 보드개발 환경 : KEIL(무료 �?��?�센스) + I-CUBE-LRWAN V2.0.0안녕하세요.RoLa개발�?� 시작한 초보 개발�?입니다.현재 UM2073 문서를 참고하여 개발�?� 진행중입니다.개발중�? low-power모드 설정하는 부분�? �?금한게 있습니다.코드�? void UTIL_LPM_EnterLowPower( void ){ UTIL_LPM_ENTER_CRITICAL_SECTION_ELP(...
HelloI noticed a strange behavior on CUBEMX when creating new project with STM32WLE5J8I MCU.When i activate a LORAWAN application and i build the project, ther's many erros of compilation but when i go to the "project manager" and "Generate files" op...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.