NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I am using demo board "NUCLEO-WL55JC1" to run SubGHz_Phy_PingPong example. if I did not change anything, I can see the message, the default usart RX and TX is PA3 and PA2.123s023:Rx start125s023:OnRxTimeout125s025:Master Tx start125s216:OnTxDon...
In the app I'm developing, I'll wind up with 50-100 files on my device's uSD card that need to be available to users on my company network. The device sits inside a sealed pressure housing and I'd really like to do this without a hard wired connectio...
Hi , Default values of the _Min_Heap_Size and _Min_Stack_Size is setting according to What? I changed these variables from 0x200 , 0x400 to 0x00 and 0x00 resprectively ,end then no problem,no error .I guess that Static and dynamic variables in RAM ar...
I am using TIM1 in the STM32WB55. I used CubeIDE and HAL to set everything up. Based on a button push I would like to update the counter period to a value in an array. I prefer not to htim1.Init.Period = period[flag]; HAL_TIM_Base_Init(&htim1)...
Hello. I programming STM32WB55 nucleo device and trying to setup printf for debugging. I have no luck so far setting it up. I have tried replacing _write in syscals.c with __attribute__((weak)) int _write(int file, char *ptr, int len){ int DataIdx; f...
How to modify the broadcast frequency of Beacon after it starts broadcasting, I follow the order:aci_gap_set_discoverable() -> Aci_gap_update_adv_data (), but does not work, else(base on BLE_HeartRate):aci_gap_set_non_discoverable () ->aci_gap_set_d...
Hi, Within the framework of a project I have to develop bluetooth beacons in order to determine the positioning of an object in interior. For that we wish to use an STM32WB in order to be used as beacons and that this one emits permanently and transm...
Hi, I'm using STM32WB55x series mcu, I wanna know how I should configure/change the relevant priority for the TIM2?In the old days we use this:void NVIC_Configuration(void) { NVIC_InitTypeDef NVIC_InitStructure; NVIC_PriorityGroupConfig(NVI...
Using an STM32WB55, timer16 for switch debounce. It is set for 100ms. I was looking in the HAL library for the timer and I see start / stop functions, etc. but how do I reset my timer after I come into the ISR? I am sure the counter will roll over...
I am trying to exchange data (str data) between two STM32 throughout Lora connectivity. Both STM32 has a lora module and the connection between them is working fine. Based on two functions:T_eError_eErrorType eDataPlane_eReceiveData_Cmd (uint32_t in_...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.