2021-05-01 8:56 PM
Hi,
I am a bit confused on the lora STM32WL sequence protocol system, I want my device to sleep and wakeup according to the periodic values I want. I have made my own sleep function (stop 2 mode & radio sleep) with wake up triggered using RTC (in seconds) and push button. Where can I put my function (PLB_SleepMode) into the sequencer utility lora end node STM32WL ?
Thank you
Here my code for custom sleep and wake up system:
void HAL_RTCEx_WakeUpTimerEventCallback(RTC_HandleTypeDef *RtcHandle)
{
//Clear wake up flag
__HAL_PWR_CLEAR_FLAG( PWR_FLAG_WU );
}
void PLB_RtcWakeUpTimeSetting( RTC_HandleTypeDef *RtcHandle, unsigned int seconds )
{
//Set wake up time
/* Disable all used wakeup source */
HAL_RTCEx_DeactivateWakeUpTimer( RtcHandle );
__HAL_RCC_WAKEUPSTOP_CLK_CONFIG( RCC_STOP_WAKEUPCLOCK_MSI );
HAL_RTCEx_SetWakeUpTimer_IT( RtcHandle, seconds - 1, RTC_WAKEUPCLOCK_CK_SPRE_16BITS );
}
RTC_HandleTypeDef *PLB_RtcPowerSavingConfig( void )
{
//Set RTC Clock, Timer, Calendar. and return RTC_HandleTypeDef to wake up
static RTC_HandleTypeDef RtcHandle;
RTC_TimeTypeDef sTime;
RTC_DateTypeDef sDate;
RtcHandle.Instance = RTC;
RtcHandle.Init.HourFormat = RTC_HOURFORMAT_24;
RtcHandle.Init.AsynchPrediv = 127;
RtcHandle.Init.SynchPrediv = 255;
RtcHandle.Init.OutPut = RTC_OUTPUT_DISABLE;
RtcHandle.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
RtcHandle.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
RtcHandle.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
HAL_RTC_Init( &RtcHandle );
sTime.Hours = 0x0;
sTime.Minutes = 0x0;
sTime.Seconds = 0x0;
sTime.TimeFormat = RTC_HOURFORMAT_24;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
HAL_RTC_SetTime( &RtcHandle, &sTime, FORMAT_BIN );
sDate.WeekDay = RTC_WEEKDAY_MONDAY;
sDate.Month = RTC_MONTH_JANUARY;
sDate.Date = 0x1;
sDate.Year = 16;
HAL_RTC_SetDate( &RtcHandle, &sDate, FORMAT_BIN );
return &RtcHandle;
}
void PLB_RtcRccPowerSavingConfig( void )
{
HAL_StatusTypeDef status = HAL_OK;
RCC_PeriphCLKInitTypeDef PeriphClkInit;
RCC_OscInitTypeDef RCC_OscInitStruct;
/* Disable backup domeain protection */
HAL_PWR_EnableBkUpAccess();
/* Enable RTC APB clock gating */
__HAL_RCC_RTCAPB_CLK_ENABLE();
/* Disable the Wake-up Timer */
__HAL_RTC_WAKEUPTIMER_DISABLE(RtcHandle);
/* In case of interrupt mode is used, the interrupt source must disabled */
__HAL_RTC_WAKEUPTIMER_DISABLE_IT(RtcHandle,RTC_IT_WUT);
__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(RtcHandle,RTC_FLAG_WUTF);
/* Get RTC clock configuration */
HAL_RCCEx_GetPeriphCLKConfig(&PeriphClkInit);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
/* COnfigure oscillator */
status = HAL_RCC_OscConfig(&RCC_OscInitStruct);
if(status == HAL_OK)
{
/* Configure RTC clock source */
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC;
status = HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit);
/* Enable RTC Clock */
if(status == HAL_OK)
{
__HAL_RCC_RTC_ENABLE();
}
}
HAL_NVIC_EnableIRQ( RTC_WKUP_IRQn );
HAL_NVIC_SetPriority( RTC_WKUP_IRQn, 1, 0 );
}
void PLB_InitSystem(void)
{
HAL_Init();
PLB_SystemClock_Config( );
SystemApp_Init();
PLB_LED_Init(PLB_LED_MODE_RUN);
PLB_LED_Init(PLB_LED_LORA_INDICATOR);
PLB_LORA_Seq_Task();
}
void PLB_PowerSavingStopMode(RTC_HandleTypeDef *RtcHandle, unsigned int WakeUpTime, GPIO_TypeDef *WakeUpGPIO)
{
GPIO_InitTypeDef GPIO_InitStructure;
Radio.Sleep();
/* Enable GPIOs clock */
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
/* Configure all GPIO port pins in Analog Input mode (floating input trigger OFF) */
/* Note: Debug using ST-Link is not possible during the execution of this */
/* example because communication between ST-link and the device */
/* under test is done through UART. All GPIO pins are disabled (set */
/* to analog input mode) including UART I/O pins. */
GPIO_InitStructure.Pin = GPIO_PIN_All;
GPIO_InitStructure.Mode = GPIO_MODE_ANALOG;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOH, &GPIO_InitStructure);
//wake up pin setting
GPIO_InitStructure.Pin = PLB_WakeupPB_GPIO_Pin; // wakeup by PA.0
GPIO_InitStructure.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStructure.Pull = GPIO_PULLDOWN;
GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init( GPIOA, &GPIO_InitStructure );
GPIO_InitStructure.Pin = GPIO_PIN_9;
GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.Pin = GPIO_PIN_8;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.Pin = GPIO_PIN_7;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, GPIO_PIN_RESET);
HAL_NVIC_SetPriority(EXTI0_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(EXTI0_IRQn);
/* Disable GPIOs clock */
__HAL_RCC_GPIOA_CLK_DISABLE();
__HAL_RCC_GPIOB_CLK_DISABLE();
__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOH_CLK_DISABLE();
//Set power saving duration by RTC
// if(WakeUpTime < 5 ) WakeUpTime = WakeUpTime + 5;
PLB_RtcWakeUpTimeSetting( RtcHandle, WakeUpTime );
// HAL_RTCEx_WakeUpTimerIRQHandler(RtcHandle);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
//Clear wake up flag
if( __HAL_PWR_GET_FLAG( PWR_FLAG_WU ) != RESET )
{__HAL_PWR_CLEAR_FLAG( PWR_FLAG_WU ); }
if(__HAL_GPIO_EXTI_GET_FLAG(GPIO_PIN_0) != RESET)
{__HAL_GPIO_EXTI_CLEAR_FLAG(GPIO_PIN_0); }
/* Enter STOP 2 mode */
LL_PWR_ClearFlag_C1STOP_C1STB();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
PLB_InitSystem();
Radio.Standby();
/*Disable all used wakeup sources: Pin1(PA.0)*/
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);
}
void PLB_SleepMode(unsigned int wakeUpTime)
{
RTC_HandleTypeDef *RtcHandle;
APP_PRINTF("\nPowerSaving Mode - Start\n");
//RCC Config for Power Saving
PLB_RtcRccPowerSavingConfig();
//RTC Config for Power Saving
RtcHandle = PLB_RtcPowerSavingConfig();
//Enter Stop Mode
PLB_PowerSavingStopMode( RtcHandle, wakeUpTime, GPIOA );
APP_PRINTF("\nPowerSaving Mode - End\n");
}
Solved! Go to Solution.
2021-05-17 4:07 AM
2021-05-17 4:07 AM
2021-06-17 5:47 AM
Hello
i made a custom board using MIDATRONICS module that integrate the STM32WLE5J8I and i don't find how to make a lorawan end node project !!! when i import the end node project from the nucleo-WL package, it doesn't work (don't make a join and don't send data!!) and because the STM32WLE5J8I HAVE ONLY 64K of flash i'm at 96% of memory !!!
Can you help please ? is anybody make a lorawan end node project directly with cubeMX for the STM32WLE5J8I without any import from the Nucleo project?
Thank you in advance
Bests Regards
2021-06-17 5:57 AM
Hi @SHATE.1 ,
please open another question as this does not relate with question above.
thank you
2021-06-17 6:04 AM
Thank you for your quick reply
i asked a question " How we can made a LORAWAN End Node application with STM32WLE5J8I ????"
can you answer please?
Thank you in advance
2021-06-17 6:16 AM
Hi,
It is always good to check the .map file to check where to spend the optimization effort,
please find some tips:
back to my comment, the question you asked does not related to "Custom sleep and wakeup system on the lora end node STM32WL"
thank you and best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.