STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Low power modes in STM32WB55 board

Hi,I am still studying about Low Power mode, according to low power run mode I tried to set V core is in range 2 and set MSI clock in 2MHz in STMWB55. please tell me how to do it?Thank You!:smiling_face_with_smiling_eyes:

Varna by Associate
  • 1382 Views
  • 2 replies
  • 0 kudos

stm32wb55 low power how to?

Good afternoon....I am new to STM32 land. I have a STM32WB55 board I am working with...I am using 16MHz internal clock source, the I2C module at 100kHz, a timer running with 8MHz and some GPIO interrupts. I would like to know how to go about placin...

SWenn.1 by Senior III
  • 1620 Views
  • 1 replies
  • 0 kudos

I am using stm32WB55, I referred example code of "BLE_HeartRateFreeRTOS". Few application specific tasks i added. In some cases if I add few statements in any of RTOS Task simply BLE don't initialize.

I am putting all application tasks in block state until successful BLE initialization, still if I add some statements or simply osDelay() in any of task, BLE is not getting on. The code execution is not even reaching to specific statement still why i...

SMane.2 by Associate II
  • 834 Views
  • 0 replies
  • 0 kudos

Resolved! Sending large amount of data with STM32WB BLE

I'm completely new to the embedded software and want to use STM32WB for my project, which will send image data from USART camera to the mobile phone. For now, I'm researching about BLE (protocols, characteristics etc.) and have no clue about how to u...

y.arikok by Associate II
  • 2999 Views
  • 2 replies
  • 0 kudos

Resolved! flashing issue on nucelo STM32WB55RGV6 revision D ?

HelloI am working on wb55RGV6 nucelo, I have bought nucleo revision C and I was able to flash it with stmcubeprogammer (stm32wb5x_FUS_fw_1_0_2.bin).I have had a new ,nucleo, a D revsion and I can't flash it, i can't delete firmware, I have tried to a...

0693W00000BbeSXQAZ.png 0693W00000BbeShQAJ.png

Resolved! BLE HeartRateMonitor FREERTOS notify problem

Dear STI'm working on a custom board, trying to adapt the BLE_HeartRateFreeRTOS to work on a STM32WB55CEU6. So far i have been able to discover and connect to the MCU and call the characteristics in the Heart Rate service:Body Sensor LocationHeart Ra...

0693W00000BbDDVQA3.png
KMeld.1 by Associate III
  • 2947 Views
  • 5 replies
  • 0 kudos

SPI reset on STM32WB55

HelloI am using an STM32WB55. This microcontroller communicates in SPI with a second STM32F4 micrcontroller.The STM32WB55 is slave and the STM32F4 is the master of communication.During an electrostatic discharge, the SPI communication is disturbed.Th...

How to take control of when the STM32WB's BLE is advertising?

To utilize the STM32WB's BLE capabilities we must enable STM32WPAN in peripherals in CUBEMX. Doing so will add the BLE template "p2p_server_app" to your project. This template by default will call APPE_Init() in your main which will in turn call the ...

TomC by Senior
  • 924 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.