NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,The ble stack provided follows BLE V5 protocol, which means that it should be possible to have multiple slaves or multiple master connections. I'm trying to build an application that would be a server/slave capable of connecting to multiple client...
I am using following snippet after the BLE Advertisement stops. I am using p2pserver example in which BLE Advertisement stops after 60 seconds and I have a timer of 65 seconds in which I have following snippet.HAL_SuspendTick();SET_BIT(PWR->CR3,PWR_C...
Hello,I'd like to debug the I2C Master/Slave example located at:..\STM32Cube\Repository\STM32Cube_FW_WB_V1.12.1\Projects\P-NUCLEO-WB55.Nucleo\Examples\I2C\I2C_TwoBoards_AdvComITI have the 2 Nucleo WB55 boards with proper I2C connection, And have a Cu...
Good day! I have 2 NUCLEO -WL55 boards. I want to use them to interrupt the charging of the device through LoRa communication. I want to use the PingPong example with a physics layer. But when I try to connect the ADC using CubeMX, the project falls ...
Multiple Zigbee examples in STM32Cube_FW_WB applications tree fail to start by triggering assertion failure in APP_ZIGBEE_ConfigEndpoints.The code under questions isstatic void APP_ZIGBEE_ConfigEndpoints(void) { struct ZbApsmeAddEndpointReqT req; ...
Hi All,I'm using the P-NUCLEO-WB55-Nucleo and I'm using all the two CPUs (CPU1 + CPU2). I must put the all board in the stop mode, I've downloaded the example PWR_EnterStopMode but I've some doubs about the manage of the CPU2 to entering in stop mod...
STM32WL RM0461 Rev 4On pages 1145 and 1146 wrote "EIE = 1 in the LPUART_CR1 register", but actually EIE in LPUART_CR3 register.
Whenever I created a new project based on LoRaWAN Skeleton, it doesn't generate MX_GPIO_Init() in any file. This requires user to write their pin configuration manually, compared to the other project that are not based on LoRaWAN Skeleton where MX_GP...
Hi,We are tying to run sigfox pushbutton app on Seeeds lora e5 module what has a stm32wl mcu built in. I have configured the radio control switch gios according to the lora e5 module and also changed the tx power define to High power. have also chang...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.