2021-08-31 9:55 AM
Good day! I have 2 NUCLEO -WL55 boards. I want to use them to interrupt the charging of the device through LoRa communication. I want to use the PingPong example with a physics layer. But when I try to connect the ADC using CubeMX, the project falls apart. I'm trying to build a project from scratch, putting together a project, connect a radio.h library, but OnTxDone, OnRxDone, OnTxTimeout, OnRxTimeout events in the subghz_phy_app.c file are not generated. Please tell me my mistake and how to connect the events
2021-08-31 10:32 AM
Find concise ADC use/configuration examples in the HAL trees, and merge those.
If CubeMX can't magic viable code you'll need to DIY.
2021-08-31 1:40 PM
But my question is that when I write a project myself, I include the radio.h library, but the OnTxDone, OnRxDone, OnTxTimeout, OnRxTimeout events in the subghz_phy_app.c file are not generated.
void SubghzApp_Init(void)
{
/* USER CODE BEGIN SubghzApp_Init_1 */
/* USER CODE END SubghzApp_Init_1 */
/* Radio initialization */
UTIL_TIMER_Create(&timerLed, 0xFFFFFFFFU, UTIL_TIMER_ONESHOT, OnledEvent, NULL);
UTIL_TIMER_SetPeriod(&timerLed, LED_PERIOD_MS);
UTIL_TIMER_Start(&timerLed);
RadioEvents.TxDone = OnTxDone;
RadioEvents.RxDone = OnRxDone;
RadioEvents.TxTimeout = OnTxTimeout;
RadioEvents.RxTimeout = OnRxTimeout;
RadioEvents.RxError = OnRxError;
Radio.Init(&RadioEvents);
Radio.SetTxConfig(MODEM_LORA, TX_OUTPUT_POWER, 0, LORA_BANDWIDTH,
LORA_SPREADING_FACTOR, LORA_CODINGRATE,
LORA_PREAMBLE_LENGTH, LORA_FIX_LENGTH_PAYLOAD_ON,
true, 0, 0, LORA_IQ_INVERSION_ON, TX_TIMEOUT_VALUE);
Radio.SetRxConfig(MODEM_LORA, LORA_BANDWIDTH, LORA_SPREADING_FACTOR,
LORA_CODINGRATE, 0, LORA_PREAMBLE_LENGTH,
LORA_SYMBOL_TIMEOUT, LORA_FIX_LENGTH_PAYLOAD_ON,
0, true, 0, 0, LORA_IQ_INVERSION_ON, true);
Radio.SetMaxPayloadLength(MODEM_LORA, BUFFER_SIZE);
Radio.SetChannel(RF_FREQUENCY);
uint8_t str=Radio.Read(0x42);
while (str == 0x00)
{
HAL_UART_Transmit(&huart1,"NoRADIO\n", 8,5);;
}
HAL_UART_Transmit(&huart1,"INIT RADIO\n", 11,5);
Radio.Rx(RX_TIMEOUT_VALUE);
UTIL_SEQ_RegTask((1 << CFG_SEQ_Task_PingPong_Process), UTIL_SEQ_RFU, PingPong_Process);
/* USER CODE BEGIN SubghzApp_Init_2 */
/* USER CODE END SubghzApp_Init_2 */
}
I can't find more information about connecting the radio library and don't know what to do.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.