NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello Every one i am using the STM32WB35CC SoC for custom BOARD, I am facing an issue that when i tries to write EEPROM I get correct response checked using Logic Analyzer but when i tried to read eeprom I GET HIGH impedance with every address. The ...
aci_hal_tone_start(..)fails for channels 3 and 4aci_hal_rx_start(..) fails for channel 3hci_le_transmitter_test(..) works on all channelshci_le_enhanced_transmitter_test(..)fails for channel 3,4,5,6hci_le_enhanced_receiver_test(..)fails for 3,4All fa...
I have been using the APP_LOG() macro from stm32_adv_trace.c to output messages while developing with the STM32WL55. This uses DMA transfers with the UART.I thought it would be useful to use the SWD debug port for console output, instead of the UART....
Hello, I am new to the STM32 world.my little board STM32 (LoRa) form ChinaST-LINK SN : 53FF6D066687505145250967ST-LINK FW : V2J38S7Board : --Voltage : 3.26VSWD freq : 4000 KHzConnect mode: NormalReset mode : Software resetDevice ID : 0x699Rev...
Is it possible to confirm the parameters and peripherals are used properly in order to work with BLE (SPBTLE) I used the MKSBOx1V1 Schematic and MX Cube and Firmware version is 1.17.0 is that is ok?
I am trying to make a simple BLE scan and advertising program which is supposed to advertise a set of changing data and scan for other devices. The advertising is completely non-connective and works as a dumb beacon, and so is the scanning. The appli...
Hello, I need to add characteristics without using the mechanism of the ioc configuration file. After only 3 (!) characteristics, the function aci_gatt_add_char( ) returns BLE_STATUS_OUT_OF_MEMORY.The available documentation is not usable to find a s...
It seems to enroll well to APP but when I try to send a message the aci_gap_init return the status value 0x46, BLE_STATUS_NOT_ALLOWED/* USER CODE BEGIN FD_WRAP_FUNCTIONS */tBleStatus P2PS_STM_App_Update_Buffer(uint16_t UUID, uint8_t *pPayload, uint8_...
Hi, We have encountered the following situation: Once the equipment is Joined to the network, if by chance there is a power cut that affects the Gateway and it restarts, we have realized that we stop receiving data from the device. Our Device can ...
I've found a significant difference in the function MX_TIMx_init() function generated from STM32 development tool for two different platforms. The first (it work) is generated for NUCLEO-F413ZH the second (it doesn't work) is generated for NUCLEO-WL5...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.