STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 302 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4120 Views
  • 0 replies
  • 3 kudos

Direct Connection Issue after Scanning

Hi there,In short I am trying to use the Nucleo-68 board to scan for Cadence Sensor devices with UUID 0x1816 which I've managed successfully. I get a list of all available devices and their addresses (double checked against a report generated through...

JakBSIP by Associate II
  • 1149 Views
  • 1 replies
  • 0 kudos

ble stack doesn't respond

Hello!In my app there are the master (stm32wb55) and up to three slaves (stm32wb55 too). In addition to this I need to scan the air permanently. At some point the ble stack of the central stops responding. It means that it becomes impossible to start...

DHunt.2 by Associate II
  • 6992 Views
  • 17 replies
  • 0 kudos

Resolved! STM32CUBEMONITOR-RF am i missing something?

Hi dark wizards of embedded electronics, its me again, javi.This time im trying to use the STM32CUBEMONITOR-RF with my STM32WB55 Nucleo pack.I cannot make it work with my NUCLEO BOARDOnce i flash the USB DONGLE (STM32WB55CGU6) with the \STM32Cube\Rep...

0693W00000DmVxWQAV.png 0693W00000DmVuOQAV.png
Javier1 by Principal
  • 1224 Views
  • 1 replies
  • 0 kudos

Need to know how to add another task in a sequencer.

I am using nucleo-stm32wb55 board, I am working on BLE peripheral and I am working on MEMS interface, I am using STM32 demo code, where OPUS is used to convert the PDM to PCM . I modified the demo code and added LCD interface and it is working, I am...

NY L.1 by Associate II
  • 2344 Views
  • 2 replies
  • 0 kudos

SIGFOX API open fails on STM32WLE5C8

Hi everyone,I have created a minimal new project for my board based on STM32WLE5C8.After enabling Sigfox into the .ioc view, in my main.c I have : HAL_Init(); SystemClock_Config(); sfx_rc_t SgfxRc = RC1; int ret = SIGFOX_API_open(&SgfxRc);However it ...

APOIR.1 by Associate II
  • 2202 Views
  • 4 replies
  • 0 kudos

Add sensors to STM32CubeWL firmware.

Let me see if I've understood. I'm using STM32CoreWL for LoRaWAN end-node implementation, where I need to insert my sensors. As specified on AN5406, the low power modes are activated by UTIL_SEQ_Idle(), when the sequencer has nothing to do. So there ...

FRest.1 by Associate III
  • 2348 Views
  • 4 replies
  • 0 kudos

rebooting in standby mode.

Hello, I am developing STM32L072.The library is using ""I CUBE LRWAN".Inside the library, I have created the part that enters the OFF mode (STANDBY mode.But the MCU doesn't consider the RTC and just keeps rebooting.What else should I consider?void PW...

SYun.2 by Associate III
  • 1954 Views
  • 3 replies
  • 0 kudos

Resolved! trying to flash coprocessor *P-NUCLEO-WB55*

Saludos!Im new to STM32W series.With two P-NUCLEO-WB55 boards on my table im trying to run the BLE_CableReplacement example.It doesnt work out of the box so i opened the readme.txt @par How to use it ?   This application requires having the stm32wb5...

0693W00000DmO1VQAV.png 0693W00000DmNxaQAF.png 0693W00000DmO5NQAV.png
Javier1 by Principal
  • 2258 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.