NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi there!I have 2 STM32WB55 Nucleo boards, both of them are having the latest FUS and Zigbee FFD fw. However, one of them cannot run as normal(another goes vey well), after downloading Zigbee_OnOff_Server_Coord sample code to it, it shows the followi...
How is the advertising data : tBleStatus aci_gap_set_discoverable( uint8_t Advertising_Type, uint16_t Advertising_Interval_Min, uint16_t Advertising_Interval_Max, ...
Hi,I'm working on a wireless application using an STM32WB55CC on a custom board. At the moment I'm stuck at flashing the wireless coprocessor firmware.Is it possible to flash the firmware via SWD using a Segger J-Link debug probe? The firmware releas...
I have a LoRa board labeled with 'MB1500-Highband-B01' and 'STM32WL55C-DK1' but no documentation. I have not found a download option for the user manual or schematic. Is it possible to obtain the User manual and schematic for this board?
Hello, I use STM32WL55 board. Now every data that I get from sensor is sent immediately. I want to accumulate data for five minutes and then send in bulk all every five minutes. I have problmes to save the data succesfully, how can I do it that micro...
I am working on the STM32WB55 Nucleo board and currently facing a problem. I have erased the whole flash, i.e. all memory locations are reset to 0xFFFFFFFF from 0x08000000 and 0x08FFFFFF. When I reconnected the board under USB DFU mode using STM32Cub...
I have been following the video to install tools and whatnot for STM32WB. So far, STM32CubeMX was installed in C:\Program Files, STM32CubeWB support was installed in a C:\Users for some reason, STM32CubeIDE was installed in C:\ST. I almost dare not c...
Hi,I have a "STM32WB55 Nucleo Pack" kit which includes a STM32WB55 nucleo board (MB1355C) and a USB DONGLE STM32WB55 (MB1293C).Today, I uploaded the "BLE_p2pServer" demo to the nucleo board and problem, nothing happens, LED2 stays green instead of bl...
I want to get this event upon connection: HCI_LE_ENHANCED_CONNECTION_COMPLETE_SUBEVT_CODE (with this data: hci_le_enhanced_connection_complete_event_rp0 )How can I do it? What should I advertise? Or is there anything else that needs to be changed f...
Slave can configure his MAC address either in the payload or internally. This I know.My question is , after connection, does the masters packets hold that (slaves) MAC address?Can Slave extract (its own) MAC address from the Masters packets?If, so ,...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.