STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

B-L072Z-LRWAN1: adding UART1 to LoRa end node project

Hello Everyone!I would really need some help. I have a B-L072Z-LRWAN1 board and I use the LoRa end node project provided by ST. I'd like to add UART1 to this project with interrupt. However, the code stops working when I initialize the UART1. Could y...

AVajd by Associate II
  • 2598 Views
  • 4 replies
  • 0 kudos

Resolved! STM32WB BLE OTA application upload

Hi,I am trying to implement the BLE OTA firmware upgrade to an existing BLE project. However before I have even looked at integrating the functionality to an existing project I am focusing on the example projects.So first up I have successfully used ...

BGrah.1 by Associate II
  • 3382 Views
  • 2 replies
  • 0 kudos

Resolved! Combining BLE Application with Existing Project

Hi all,I have been working on a Nucleo 68 board to develop firmware for my project. I have been working in parallel on two projects - one was purely hardware control - read/write to/from various peripheral devices (UART with IT and I2C DMA and Extern...

JakBSIP by Associate II
  • 4265 Views
  • 5 replies
  • 0 kudos

How to extract sensor values from PWM signal?

Hi everyone. I connected the SDS011 Dust Sensor with my Nucleo WL55JC1 via UART and I am receiving my sensor data. According to the Sensor data sheet the values can be also provided as output in PWM form on the certain pin.In order to achieve this I ...

0693W00000FC9btQAD.jpg
MStew.1 by Associate III
  • 1477 Views
  • 3 replies
  • 0 kudos

i-cube_lrwan_v2.1.0(using NUCLEO-L452re and I-NUCLEO-LRWAN1)

I own a NUCLEO-L452re and I want to implement LoRa communication using I-NUCLEO-LRWAN1 (with SX1272 transceiver).Is it okay to program in STM32CubeIDE by using sx1272mb2das and NUCLEO-L476RG in i-cube_lrwan ?i-cube_lrwan_v2.1.0\STM32CubeExpansion_LRW...

Kdohy.1 by Associate
  • 1165 Views
  • 1 replies
  • 0 kudos

SUBGHZ_Radio_IRQHandler Interrupt deadlock

Hi. I have a floating problem with subghz module interrupts. In case of interrupt caused when MCU works with SUBGHZ module deadlock happened, because periph are locked by previous operation and we can't read interrupt status register of subghz. Is th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.