NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I tried to debug the code by changing the "CFG_DEBUGGER_SUPPORTED" to 1 , but still we are facing the issues, RTOS tasks are not executing as expected. We found some task in ble_app.c with priority of "osPriorityNone" which is 0. Does this example co...
In the video workshop, it changes the led blinking frequency after the ble connection with mobile app. But I am still confused with how to send the data to PC. For example, if I want to send "Hello word" to my computer, where should I put this code a...
Dear Community!After my unsuccessful question and updating the library, I managed to quite quickly and simply transfer the "123 ..." data and see it on the gateway.The gateway has the ability to send packets in response. It contains parameters port n...
hi community, i'm getting trouble in updating firmware over the air via BLE, i followed the AN5247 for updating firmware via ST BLE SENSOR APP but it didn't work properly. I'm not able to load the new firmware in my nucleo, the board doesn't seems to...
We are trying to load the stm32wb5x_Zigbee_FFD_fw.bin on STM32WB55RC, but the address table in the release note show as 0x00 for FFD stack and STMCube Programmer gives error as bad address.What is the actual address for Zigbee stack for 256K Flash de...
Hello,I was just wondering whether it was possible to form a 2M PHY connection with a Windows BLE App?I have developed firmware for my STM32WB nucleo board, along with a C#.NET Windows application to connect with it.I am trying to maximise throughput...
I am trying to transmit a single int using LoRa and the SUBGHZ_PHY middleware. However, I am unsure as to why UART has to be configured under 'Platform Settings', and how I can setup the STM project for this purpose. I am using STM32CubeIDE, and a Nu...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.