STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

About I2C communication using STM32WL. STM32WLを使用�?��?�I2C通信�?��?��?��?�。

I want to use RTC (RX-8571) for I2C communication with STM32WLE5JC. I wrote the code using [HAL_I2C_Master_Transmit] and [HAL_I2C_Master_Receive], but I can only send the device address of the first byte. The errata says "Write the first data in I2C_...

Resolved! STM32CubeMX , how to live with it

I'm trying to set configuration for STM32WL55JC but I have no luck at all. I have set some pins, namely inputs: PB1,PC6,PC13, outputs: PB10,11,15, pc3,4,5, but the problem is all the time, I'm trying to not to touch almost anything wht is not needed...

Join fail for P-Nucleo-Lrwan2 to gateway

Hi Folks,Newbie at this. Bought P-Nucleo-Lrwan2 last week and have issue with join. Pack comes with L073Rz and I-NUCLEO-LRWAN1 ARDUINO expansion board used as a sensor node. Flashed STM32CubeExpansion_LRWAN_V2.1.0 with NUCLEOL073RZ, AT_Master but sti...

KLow.1 by Associate
  • 1095 Views
  • 0 replies
  • 0 kudos

tiny_lpm documentation? Exit stop mode causing issues.

I have built an app based on the p2p server. I have added several tasks to read adc, drive pwm an talk to i2c devices. The app runs as expected when I disable the stop mode.UTIL_LPM_SetStopMode(1 << CFG_LPM_***, UTIL_LPM_DISABLE);However when I all...

LHarm.1 by Associate III
  • 1338 Views
  • 0 replies
  • 0 kudos

NUCLEO-WL55J STM32WL Flash Erasing failed after loading the BFU_LoRaWAN_End_Node.bin Please share your inputs to disable the flash write protection.

I have used STM32Cube_FW_WL_V1.1.0 -> LoRaWAN_FUOTA -> 1_Image sample and build the binary file ->  BFU_LoRaWAN_End_Node.binAfter flashing the binary, STM32WL66 Option Bytes got changed and i could not able to erase and update the fflash after that. ...

HVeer.1 by Associate II
  • 2081 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.