NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hey thereI'm working with stm32wb with custom board, I have two strange issues.I'm tying to probe GPIO_IOToggle example but the program only run when i charge the code or when I debugged it with STM32CUBEIDE, whne i press reset or activate the source...
Helloi made a custom board using MIDATRONICS module that integrate the STM32WLE5J8I and i don't find how to make a lorawan end node project !!! when i import the end node project from the nucleo-WL package, it doesn't work (don't make a join and don'...
Hello,I am using the STM32WB55 Nucleo board and have gone through a few of the example applications. I would now like to create my own BLE application similar to the heart rate monitor. I really am not sure how to start and was hoping for a decent ...
Hello,We are designing a PCB based on the NUCLEO-WL55JC boardWe are looking for the Altium project files.Someone can share a link?Thanks.BEEPH
Dear ST communityI've been trying to implement the BLE_RfWithFlash example from the STM32WBCube package into my BLE application.When trying to write/erase flash, the MCU disconnects the BLE client and triggers a hard fault. If I run the application i...
Looking at the HearRate Example with RTOS.I see that user app holds all the handlers in :PLACE_IN_SECTION("BLE_DRIVER_CONTEXT") static HRS_Context_t HRS_Context;What is the purpose of this placement?Can it be changed to a simple static?thanks
Hi all,We are using stm32 PDM to PCM library to convert PDM mic data into PCM data. On that we had an option to control the mic gain from -12db to 51db as mentioned in data sheet.So we try to increase the db level, But we cannot able to increase the ...
Hi, I currently have a STWINKT1B board flashed with the predictive maintenance sample application. This allows me to connect my board to the BLE sensor app through Bluetooth and it also allows me to log the ACCELLEROMETER sensor values to MQTT. Howev...
Hi. I started a new project with the STM32WB35CEU as the target. Both in the datasheet and cubeMX MCU info it states 512Kbytes FLASH and 96KBytes of RAM.But when I generate that project code with cubeMX the linkerscript shows 256KFLASH (rx) : ORIGIN...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.