STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB Bluetooth and ZigBee Mesh Webinar Part1

Thanks for your participation to the STM32WB Bluetooth and ZigBee Mesh Webinar .Recording of the session is here.Following is a collection of questions received during the Q&A session we were unable to answer in real time due to time constrains.For d...

Resolved! Append uint32 to string for BLE local name

I think this is more of a c programming question rather than a MCU question, but I figured I would ask anyway. I am trying to append the chip ID from an STM32WB onto the BLE local name for my application and am having trouble figuring out how to do ...

kcire L. by Associate III
  • 1829 Views
  • 2 replies
  • 0 kudos

Resolved! Differences between NUCLEO-WL55JC1 and NUCLEO-WL55JC2 ?

What are the physical differences between NUCLEO-WL55JC1 and NUCLEO-WL55JC2 Dev boards.Is it possible to convert the NUCLEO-WL55JC2 to a NUCLEO-WL55JC1?The NUCLEO-WL55JC1 seems to be unavailable on the market at this point.

TV by Associate II
  • 2514 Views
  • 2 replies
  • 1 kudos

Can B-L072Z-LRWAN1 Build A Lora Network?

The  B-L072Z-LRWAN1 has two examples: ClassA and PingPong. ClassA requires a Multitech Gateway which is expensive, PingPong only for two nodes.If I have 3 to 10 long range nodes, plan to do star network, One node is master and others are slave, can...

WB5MMG RTC Inaccurate

WB5MMG RTC Inaccurate, RTC increase by 1s requires 10s or more in reality.32.768 LSE has been used. RTC_TimeTypeDef sTime = {0}; HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN); RTC_DateTypeDef sDate = {0}; HAL_RTC_GetDate(&hrtc, &s...

0693W00000HpcCBQAZ.png 0693W00000HpcCeQAJ.png
Csu.11 by Associate II
  • 3407 Views
  • 7 replies
  • 0 kudos

STM32wl55 subghz linker error using cubemx

Hi there,I want to run some commands and get results on our custom designed STM32wl55 PCB. I started the project using cubemx but there is a subghz linker error.Could you please help me how to solve it?ThanksError: L6218E: Undefined symbol HAL_SUBGHZ...

SK.20 by Associate
  • 4621 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.